Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Battery for stepper motors and controller
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 3 answers
  • Subscribers 328 subscribers
  • Views 5110 views
  • Users 0 members are here
  • controller
  • hardware
  • open_source
  • power_supply
  • regulated_power
  • stepper_motors
Related

Battery for stepper motors and controller

balearicdynamics
balearicdynamics over 10 years ago

Hi to all. The scenario is the following: by one side there is a couple of stepper motors (running on 4.5 Vcc.) and by the other there is the 5 Vcc needed to power the controller board (consuming very few current, i.e. 150 mA). So, there will be two different power lines. To get them from a single battery (e.g. 2A LiIon rechargeable battery), is it sufficient splitting the battery power supply, one to the motors and one to a 5V power regulator to power the controller?

 

Thank you in advance image Enrico

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz +3
    Shabaz, I attach three images of the kind of batteries that I mean. Not super powerful but I know them very well and are very realiable. Voltage is 7.2 V that is ideal for 5V (or 3V) based devices and…
  • shabaz
    shabaz over 10 years ago +1 suggested
    Hi Enrico! That does work, but sometimes people do have issues with it because of noise or volt drop. Motor power varies a lot too since they are so diverse. An electrolytic cap very close to the motors…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz +1
    Hi Shabaz Thank you for your answer and precious support. Your blog post is one that I followed during a period that from here was impossible to like and bookmark. In this project I will use camera batteries…
Parents
  • D_Hersey
    0 D_Hersey over 10 years ago

    I know I am of a minority opinion on this, around here, but I recommend establishing an isolation boundary between your logic circuit and your motor circuit, such as optoisolatorors.  This way you can worry less about spikes.  Who knows the future?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 10 years ago

    I know I am of a minority opinion on this, around here, but I recommend establishing an isolation boundary between your logic circuit and your motor circuit, such as optoisolatorors.  This way you can worry less about spikes.  Who knows the future?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to D_Hersey

    This sounds good. To be honest I also though to this option but the entire project will be supported with relatively low power motors, i.e. 5 V 1A max steppers Nema 17 1.8 Deg 200 steps per rotation with a torque of about 2 Kg. The main board will be PSoC4 that hss a reasonable number of well designed protections so I am not sure if adopting optocouplers maybe worthy or not.

     

    Where do you suggest to put the optoisolators ?

     

    Enrico