Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Battery for stepper motors and controller
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 3 answers
  • Subscribers 328 subscribers
  • Views 5039 views
  • Users 0 members are here
  • controller
  • hardware
  • open_source
  • power_supply
  • regulated_power
  • stepper_motors
Related

Battery for stepper motors and controller

balearicdynamics
balearicdynamics over 10 years ago

Hi to all. The scenario is the following: by one side there is a couple of stepper motors (running on 4.5 Vcc.) and by the other there is the 5 Vcc needed to power the controller board (consuming very few current, i.e. 150 mA). So, there will be two different power lines. To get them from a single battery (e.g. 2A LiIon rechargeable battery), is it sufficient splitting the battery power supply, one to the motors and one to a 5V power regulator to power the controller?

 

Thank you in advance image Enrico

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz +3
    Shabaz, I attach three images of the kind of batteries that I mean. Not super powerful but I know them very well and are very realiable. Voltage is 7.2 V that is ideal for 5V (or 3V) based devices and…
  • shabaz
    shabaz over 10 years ago +1 suggested
    Hi Enrico! That does work, but sometimes people do have issues with it because of noise or volt drop. Motor power varies a lot too since they are so diverse. An electrolytic cap very close to the motors…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz +1
    Hi Shabaz Thank you for your answer and precious support. Your blog post is one that I followed during a period that from here was impossible to like and bookmark. In this project I will use camera batteries…
Parents
  • D_Hersey
    0 D_Hersey over 10 years ago

    It is a little more expensive to implement because now another supply is needed, it is more trouble, more space and more money.  The consumer market gets some rather poor circuits because the market is so cost-sensitive.  Optoisolators and similar circuits are fairly ubiquitous in medical electronics, for example, because the market is professional and not so hyper-reactive to cost.  These are interesting circuits.  I am not telling you to use them so much as to encourage you to read the highly-rewarding application notes about them, then decide for yourself.  They have products nowadays called 'logic optoisolators' that require a minimum of design effort to implement. Opto-isolators are a little less popular now because bandwidth and circuits they protect are a little more robust by nature now.  There are other forms of isolators that use acoustic or RF energy instead of light that are used in special cases.  Transformers can also be used in some cases to minimize the energetic transfer across a barrier.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 10 years ago

    It is a little more expensive to implement because now another supply is needed, it is more trouble, more space and more money.  The consumer market gets some rather poor circuits because the market is so cost-sensitive.  Optoisolators and similar circuits are fairly ubiquitous in medical electronics, for example, because the market is professional and not so hyper-reactive to cost.  These are interesting circuits.  I am not telling you to use them so much as to encourage you to read the highly-rewarding application notes about them, then decide for yourself.  They have products nowadays called 'logic optoisolators' that require a minimum of design effort to implement. Opto-isolators are a little less popular now because bandwidth and circuits they protect are a little more robust by nature now.  There are other forms of isolators that use acoustic or RF energy instead of light that are used in special cases.  Transformers can also be used in some cases to minimize the energetic transfer across a barrier.