Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum LiPo 3.3V Linear Regulation - Chip Suggestions?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 327 subscribers
  • Views 3827 views
  • Users 0 members are here
Related

LiPo 3.3V Linear Regulation - Chip Suggestions?

jgreenb8@gmail.com
jgreenb8@gmail.com over 10 years ago

Greetings,

 

I'm working with a design I developed and I'm running into the shortcomings of Inductor based regulators. I'm trying to regulate a 3.7V nom. lipo battery to 3.3V for ADC sampling of a strain gauge bridge. Unfortunately I am running into issues with noise and I believe it's due to the oscillations of the voltage regulator I am currently using, the TI TPS61200.

 

Does anyone know of a good linear voltage regulator that can take the 3.7-4.2 V of a LiPo and still hold a 3.3V stable output? 

 

I've searched for some time and I am not having much luck. Perhaps I am thinking of this from the wrong approach.

 

Many Thanks!

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Jacob Greenburg,

         https://www.circuitsathome.com/dc-dc/designing-dc-dc-converters-using-ti-tps61200-controller  is a good read. But I see the current starts at 1500 mA and ends just at ~800 mA at discharge of LiPo which should NOT go below 2.7V. I hope you did not go below and reverse the polarity on the LiPo. Since the current is variable when the voltage held at 3.3 V you should expect the current to drop. If noise is the problem look at http://www.ti.com/product/tps62230 . In the description you can force PWM mode that will lower noise . But this can handle only 500 mA!image

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    Jacob Greenburg,

         https://www.circuitsathome.com/dc-dc/designing-dc-dc-converters-using-ti-tps61200-controller  is a good read. But I see the current starts at 1500 mA and ends just at ~800 mA at discharge of LiPo which should NOT go below 2.7V. I hope you did not go below and reverse the polarity on the LiPo. Since the current is variable when the voltage held at 3.3 V you should expect the current to drop. If noise is the problem look at http://www.ti.com/product/tps62230 . In the description you can force PWM mode that will lower noise . But this can handle only 500 mA!image

     

    Clem