Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Any affordable mini computer available in the market?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 326 subscribers
  • Views 1417 views
  • Users 0 members are here
  • raspberry
  • minicomputer
  • robot
  • affordable
  • microcontroller
  • iot
  • arduino
  • business
  • hacking
Related

Any affordable mini computer available in the market?

e14 Contributor
e14 Contributor over 10 years ago

Well, I am a noob in this electronic kind of stuff but have an idea in my mind. What I'm planning is make a mini-computer using any microcontrollers like the Arduino Uno board or the Raspberry Pi (may be 2 or 3).

What if we make a mini-computer, no matter with Arduino board or maybe raspberry, And try to bring it in the market?

Will it bring or cause any violation rights or something? I mean will it be illegal if I make a mini-computer with any of the existing microcontrollers and bring my mini-computer in the market to sell it?

And if no, then any ideas for making one which is NOT a common one?

Thanks in Advance!

  • Sign in to reply
  • Cancel
Parents
  • amgalbu
    0 amgalbu over 10 years ago

    raspberry, arduino & c are open source hardware projects. In general, there are two broad classes of open-source licenses: copyleft and permissive. Copyleft licenses (also referred to as “share-alike” or “viral”) are those which require derivative works to be released under the same license as the original; common copyleft licenses include the GNU General Public License (GPL) and the Creative Commons Attribution-ShareAlike license. Other copyleft licenses have been specifically designed for hardware; they include the CERN Open Hardware License (OHL) and the TAPR Open Hardware License (OHL). Permissive licenses are those which allow for proprietary (closed) derivatives; they include the FreeBSD license, the MIT license, and the Creative Commons Attribution license. Licenses that prevent commercial use are not compatible with open-source; see this question for more.

    Please note that the open-source hardware definition is not a license, although it does describe some of the license terms which are compatible with the practice of open-source hardware.

    (From oshw site)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • amgalbu
    0 amgalbu over 10 years ago

    raspberry, arduino & c are open source hardware projects. In general, there are two broad classes of open-source licenses: copyleft and permissive. Copyleft licenses (also referred to as “share-alike” or “viral”) are those which require derivative works to be released under the same license as the original; common copyleft licenses include the GNU General Public License (GPL) and the Creative Commons Attribution-ShareAlike license. Other copyleft licenses have been specifically designed for hardware; they include the CERN Open Hardware License (OHL) and the TAPR Open Hardware License (OHL). Permissive licenses are those which allow for proprietary (closed) derivatives; they include the FreeBSD license, the MIT license, and the Creative Commons Attribution license. Licenses that prevent commercial use are not compatible with open-source; see this question for more.

    Please note that the open-source hardware definition is not a license, although it does describe some of the license terms which are compatible with the practice of open-source hardware.

    (From oshw site)