Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum How is this RS485 module working?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 329 subscribers
  • Views 1525 views
  • Users 0 members are here
  • rs485
Related

How is this RS485 module working?

rishi2628
rishi2628 over 10 years ago

I am using an RS485 module :- http://www.elecrow.com/uart-ttl-to-rs485-twoway-converter-p-1545.html

This module is bidirectional and uses a single pair of differential signal to transmit/receive data. My question is how is the chip deciding whether it has to transmit data from TX to A+ B- or from A+ B- to RX?. Shouldn't there be 2 pairs of differential signal, one pair for TX and the other pair for RX? What is happening in this module??

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 10 years ago in reply to johnbeetem +2
    The clue is probably the diode in the middle. My guess would be a simple re-triggerable monostable (Schottky diode, cap and resistor) running from the transmit data to control the transceiver's direction…
  • johnbeetem
    johnbeetem over 10 years ago +1
    RS-485 is usually a half-duplex protocol with a single master and multiple slaves sharing a single A+B- differential pair. The master sends out a "poll" request and then disables its transmitter while…
  • gadget.iom
    gadget.iom over 10 years ago in reply to johnbeetem +1
    Hi johnbeetem I didn't want to add too much detail to yet another of these open-ended questions. But as this thread now has parties worth communicating properly with... I completely agree with your counterfeit…
Parents
  • COMPACT
    0 COMPACT over 9 years ago

    RS485 uses 4 wires for unrestricted full-duplex mode.

    However just two wires can be used for half-duplex mode between two nodes which can be made to appear as a (slower) full duplex connection to their hosts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • COMPACT
    0 COMPACT over 9 years ago

    RS485 uses 4 wires for unrestricted full-duplex mode.

    However just two wires can be used for half-duplex mode between two nodes which can be made to appear as a (slower) full duplex connection to their hosts.