Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Open Source options for RGB to HDMI
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 326 subscribers
  • Views 8449 views
  • Users 0 members are here
Related

Open Source options for RGB to HDMI

baldengineer
baldengineer over 5 years ago

For my Mini Apple IIe project, I'd like to include HDMI output. This project is a one-off. So, I want HDMI to work, but I am not worried about passing compliance or licensing tests.

 

Ideally, I'd like to find an off-the-shelf chip that can take analog RGB signals, a sound input, and convert them to HDMI.

 

Why not DVI? The sound. From what I understand, DVI does not support a sound channel.

 

Looking around at the obvious semiconductor companies, it seems like analog-RGB to HDMI is something that exists. However, all require contact for more information. I suspect this step is to make sure you are licensed for HDMI IP. Fair step, but I am not selling anything.

 

On the grey market, I found the IT6613 (mirrored datasheet). It is used in the Open Source Scan Converter project. An interesting chip, it seems to do what I want, but it is huge and has a bunch of stuff I don't need.

 

I suppose one option is to do something with an FPGA. But I was really hoping to find something off-the-shelf.

 

I briefly looked at the Pi Pico PIO DVI implementation. But, again, the sound seems to be a stumbling point there.

 

Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 5 years ago +3
    Something like this in chip form? https://www.ebay.ca/itm/144137191329?hash=item218f3effa1:g:t3oAAOSwZrhhCK5L
  • baldengineer
    baldengineer over 5 years ago in reply to dougw +3
    It is an interesting idea. That takes Component video which is Luma-based. I have considered buying something similar that takes in RGB, and tearing it apart. There is probably a cheap SCART-to-HDMI adapter…
  • baldengineer
    baldengineer over 5 years ago in reply to wolfgangfriedrich +3
    Excellent find Wolfgang! With a brief look, I believe this is what I am after. I'll investigate the datasheet a bit more later. It does look like there are a few suppliers on the grey market that offer…
Parents
  • wolfgangfriedrich
    0 wolfgangfriedrich over 5 years ago

    A combination of Analog Device's AD9983 + ADV7513 might work.

    Both chips seem to have limited supply at some distributors. The AD9983 is not recommended for new designs, but from your former posts, your project isn't exactly new either. image

    And I am not sure how much configuration those chips need to make them do what you want.

    - W.

    PS: I was looking at those chips for a composite video to HDMI solution, but that would need another step of composite to RGB first and I never prototyped it. And if it is really a one-off, you can always buy an eval board and 'borrow' the chip from there.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • baldengineer
    0 baldengineer over 5 years ago in reply to wolfgangfriedrich

    I initially came across the ADV7513. But lack of access to (real) datasheet is what made me realize I might not be able to gain access to the resources I need.

     

    As I think about your suggestion, though, I might be able to skip the ADC. The signals I get from the MEGA-II are a digital RGB sequence. So, I can probably skip converting it to analog just to get them converted back to digital. I will, probably, need to change the digital RGB sequence I get into something a chip like the ADV7513 understands.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • baldengineer
    0 baldengineer over 5 years ago in reply to wolfgangfriedrich

    I initially came across the ADV7513. But lack of access to (real) datasheet is what made me realize I might not be able to gain access to the resources I need.

     

    As I think about your suggestion, though, I might be able to skip the ADC. The signals I get from the MEGA-II are a digital RGB sequence. So, I can probably skip converting it to analog just to get them converted back to digital. I will, probably, need to change the digital RGB sequence I get into something a chip like the ADV7513 understands.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • wolfgangfriedrich
    0 wolfgangfriedrich over 5 years ago in reply to baldengineer

    baldengineer 

    With digital RGB, this one might be an option:

    Chrontel CH7035. I can't look at more details right now, because it is hosted in China, but there is a project over at Hackaday.io that uses the chip and might be able to be reverse engineered.

    https://hackaday.com/2019/07/26/hdmi-from-your-arduino/

    Buying one might be a challenge too.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • baldengineer
    0 baldengineer over 5 years ago in reply to wolfgangfriedrich

    Excellent find Wolfgang! With a brief look, I believe this is what I am after. I'll investigate the datasheet a bit more later.

     

    It does look like there are a few suppliers on the grey market that offer them. Not my preferred acquisition method, but I probably have no other choice in this case.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wolfgangfriedrich
    0 wolfgangfriedrich over 5 years ago in reply to baldengineer

    Yeah, findchips.com only shows one German distributor, that only sells full trays of 168 pieces. If you want to go into mass production, I could help with the translation. image

    • Cancel
    • Vote Up +3 Vote Down