Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum I need help with creating 1 KHz, +/- 12V PWM signal.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 328 subscribers
  • Views 4002 views
  • Users 0 members are here
  • j1772
  • parallax
  • pwm
  • diy
  • basic_stamp
  • evse
Related

I need help with creating 1 KHz, +/- 12V PWM signal.

DarkStar
DarkStar over 15 years ago

I'm working on building my own EVSE (Electric Vehicle Supply Equipment) that is SAE J1772-2010 compliant. Unfortunately generating the control pilot signal is a bit more complicated than blinking an LED or reading an RFID tag, so I need some help.

 

The basic equipment I'm already using includes a 12 volt DC power supply, powering a Parallax Super Carrier Board with a BASIC 2 Stamp. I'm using the microcontroller to read an RFID tag and display information on an LCD display.

 

The element I'm missing is some way to generate a 1 KHz, +/- 12V PWM square wave signal, whose duty cycle is controlled by the BASIC 2 Stamp. For example, a 8% duty cycle will let the vehicle know it can draw 6 amps, 20% draws 12 amps. The recommend frequency tolerance and duty cycle tolerance is ±2%. Attached is the technical document on J1772 if it helps describe things a bit clearer!

 

I'll be documenting my project here and on the MyNissanLeaf.com forum so that others can take advantage of what I learned by going through the process, so any help is greatly appreciated!

Attachments:
imageSAE J1772-2010 SAE Electric Vehicle and Plug in Hybrid Electric Vehicle Conductive Charge Coupler.pdf
  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 15 years ago

    Get a PIC PIC12F683T-I/SNPIC12F683T-I/SN and have it output a PWM signal. It can also read inputs from the Stamp.

     

    /*
    * PWM registers configuration
    * Fosc = 4000000 Hz (4MHz)
    * Fpwm = 1000.00 Hz (Requested : 1000 Hz)
    * Duty Cycle = 2 %
    * Resolution is 10 bits
    * Prescaler is 4
    * Ensure that your PWM pin is configured as digital output
    */
    PR2 = 0b11111001 ;
    T2CON = 0b00000101 ;
    CCPR1L = 0b00000100 ;
    CCP1CON = 0b00111100 ;

     

    Then boost the output to 12V.

     

    An option.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DarkStar
    0 DarkStar over 15 years ago in reply to Catwell

    Wow, well the price tag for a development kit and the learning curve are both a bit high (for me) for the PIC12F683T-I/SNPIC12F683T-I/SN. Is there a way to do this without using yet another microcontroller?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to DarkStar

    Get an Olimex PIC-P8 http://www.olimex.com/dev/pic-p14.html dev board. It's $10 USD.

    Then get the PIC12F683 for $1.29 USD.

     

    This will be a $12 dollar endeavour.

     

    Below is a PIC-P18 I have with a PIC16F1827 for a project I am working on. It's very similar to the above one. The 16F series has a few more features, you may also want to toy with this as well.

    image

     

    Expanding your knowledge of embedded development is important. Give PIC a try.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Catwell
    0 Catwell over 15 years ago in reply to DarkStar

    Get an Olimex PIC-P8 http://www.olimex.com/dev/pic-p14.html dev board. It's $10 USD.

    Then get the PIC12F683 for $1.29 USD.

     

    This will be a $12 dollar endeavour.

     

    Below is a PIC-P18 I have with a PIC16F1827 for a project I am working on. It's very similar to the above one. The 16F series has a few more features, you may also want to toy with this as well.

    image

     

    Expanding your knowledge of embedded development is important. Give PIC a try.

     

    Cabe