Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum I need help with creating 1 KHz, +/- 12V PWM signal.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 328 subscribers
  • Views 4005 views
  • Users 0 members are here
  • j1772
  • parallax
  • pwm
  • diy
  • basic_stamp
  • evse
Related

I need help with creating 1 KHz, +/- 12V PWM signal.

DarkStar
DarkStar over 15 years ago

I'm working on building my own EVSE (Electric Vehicle Supply Equipment) that is SAE J1772-2010 compliant. Unfortunately generating the control pilot signal is a bit more complicated than blinking an LED or reading an RFID tag, so I need some help.

 

The basic equipment I'm already using includes a 12 volt DC power supply, powering a Parallax Super Carrier Board with a BASIC 2 Stamp. I'm using the microcontroller to read an RFID tag and display information on an LCD display.

 

The element I'm missing is some way to generate a 1 KHz, +/- 12V PWM square wave signal, whose duty cycle is controlled by the BASIC 2 Stamp. For example, a 8% duty cycle will let the vehicle know it can draw 6 amps, 20% draws 12 amps. The recommend frequency tolerance and duty cycle tolerance is ±2%. Attached is the technical document on J1772 if it helps describe things a bit clearer!

 

I'll be documenting my project here and on the MyNissanLeaf.com forum so that others can take advantage of what I learned by going through the process, so any help is greatly appreciated!

Attachments:
imageSAE J1772-2010 SAE Electric Vehicle and Plug in Hybrid Electric Vehicle Conductive Charge Coupler.pdf
  • Sign in to reply
  • Cancel
Parents
  • Bassman59
    0 Bassman59 over 15 years ago

    Assuming you can generate the square wave, use an op-amp level shifter to boost the square wave amplitude to +/-12V.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Bassman59
    0 Bassman59 over 15 years ago

    Assuming you can generate the square wave, use an op-amp level shifter to boost the square wave amplitude to +/-12V.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Catwell
    0 Catwell over 15 years ago in reply to Bassman59

    BOOM!

    image

     

    Cabe