Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Large, flat, flexible waterproof button?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 329 subscribers
  • Views 1395 views
  • Users 0 members are here
  • bluetooth
  • audio
  • button
  • waterproof
Related

Large, flat, flexible waterproof button?

jmsaltzman
jmsaltzman over 15 years ago

I'm working on a ski helmet audio project, with a stereo bluetooth headset (Motorola S305) circuit wired in.

 

I'd like to have large buttons on the outside of the helmet, to be activated by gloved fingers.

 

The buttons are the trickiest part since they'd have to be big, stick securely to the helmet, and resistant to moisture.

 

I saw Ben Heck wire buttons under foam on a microphone, which is nice since it sidesteps making a button from scratch.

I also found this thread which suggests using sticky foam pads and tin foil:

http://forums.benheck.com/viewtopic.php?f=20&t=23041

 

I'm curious about people's experiences with different types of foam, esp. foam that might be waterproof.  I also wonder about making a sandwich of foam and (a) foil with a spring of some kind or (b) an off-the-shelf button and coating it all, maybe in latex, to seal it up.

 

Any suggestions would be most appreciated!


Thanks,

-Jeff

jmsarduino.blogspot.com

  • Sign in to reply
  • Cancel
  • Catwell
    0 Catwell over 15 years ago

    Jeff,

     

    Although this one is small, you might want to look into water tight limit switches : E14 product # 25C443025C4430

     

    I use them on CNC machinery that are often soaked in coolant, oils, and other liquids. They work great for me, and they are simple NC/NO contact switches.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jmsaltzman
    0 jmsaltzman over 15 years ago in reply to Catwell

    Interesting buttons!  Thanks for the info.  I need something flat though, with a large area, that can stick to the rounded surface of the helmet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to jmsaltzman

    In that case, start looking at membrane switches.

     

    Or place one of the water tight switches into a E-Stop E-Stop. It would be hilarious to have a big red button on the side of your helmet.

     

    Does the switch have to be on the side, or outside of your helmet? How about under near the chin? You could activate it with your chin or hand. The aforementioned water tight switches are very small and could be tucked anywhere.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jmsaltzman
    0 jmsaltzman over 15 years ago in reply to Catwell

    Membrane switches generally need a good amount of concentrated force and are usually close together.  I want to operate the buttons with my gloves on, so think of a button easily pressed with a small pillow that doesn't stick out too far from the rounded surface it's mounted to.

     

    Chin buttons wouldn't work well for what I'm aiming for, since I'll need seven buttons:

    1. pause/play
    2. phone (answer, hang up, voice command)
    3. volume up
    4. volume down
    5. next track
    6. previous track
    7. power

     

    I have a pair of Motorola S805 headphones, with three buttons on each ear piece, so I think I'll use their arrangement or something close to it:

    • Left side: phone button (centered), with volume up and down above it, next to each other.
    • Right side: pause/play button (centered), with next track and previous track above it, next to each other.
    • Power button on the back of the helmet, above the edge.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I used some thin white flexible (I think PE) protective wrapping foam to replace defective foam from a car horn switch - the basic configuration was metal plate with nubs , foam insert with holes for the nubs, metal plate.  The foam was about 1/8 to 3/16 thick, and compressed enough without a great deal of force for the metal to make contact.

     

    The plastic wrapping foam was totally waterproof - a good choice of metal might be important if it wasn't enclosed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jmsaltzman
    0 jmsaltzman over 15 years ago

    I came up with a good solution using a stack of adhesive-backed craft foam pieces, cut to surround a clicky 12mm square button in a sort of stepped pyramid.  The bottom piece of foam stuck very well to the helmet surface, and foam above that which didn't stick as well to the foam below got a bead of hot glue around the edge.  They're plenty water-proof since I hot glued any place water could get in.  A small Case Logic hearing aid case attached to the goggle strap on the rear of the helmet holds the electronics-- bluetooth board, connections, battery and charger circuit; appropriate since it's a sort of hearing aid image

     

    The project is complete and the helmet has had two glorious, rocking days out on the slopes.  It works just like I'd hoped, giving me full remote control of my iPhone with gloved hands while flying down the mountain.  I got plenty of funny looks and people asking "what's up with your  helmet?"

     

    I'll post pictures and a demo video soon, thanks for the replies!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to jmsaltzman

    Jmsaltzman,

     

    Post pictures and schematics of what your final design ended up being.

     

    Looking forward to it.

     

    Cabe