Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Large, flat, flexible waterproof button?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 329 subscribers
  • Views 1409 views
  • Users 0 members are here
  • bluetooth
  • audio
  • button
  • waterproof
Related

Large, flat, flexible waterproof button?

jmsaltzman
jmsaltzman over 15 years ago

I'm working on a ski helmet audio project, with a stereo bluetooth headset (Motorola S305) circuit wired in.

 

I'd like to have large buttons on the outside of the helmet, to be activated by gloved fingers.

 

The buttons are the trickiest part since they'd have to be big, stick securely to the helmet, and resistant to moisture.

 

I saw Ben Heck wire buttons under foam on a microphone, which is nice since it sidesteps making a button from scratch.

I also found this thread which suggests using sticky foam pads and tin foil:

http://forums.benheck.com/viewtopic.php?f=20&t=23041

 

I'm curious about people's experiences with different types of foam, esp. foam that might be waterproof.  I also wonder about making a sandwich of foam and (a) foil with a spring of some kind or (b) an off-the-shelf button and coating it all, maybe in latex, to seal it up.

 

Any suggestions would be most appreciated!


Thanks,

-Jeff

jmsarduino.blogspot.com

  • Sign in to reply
  • Cancel
Parents
  • jmsaltzman
    0 jmsaltzman over 15 years ago

    I came up with a good solution using a stack of adhesive-backed craft foam pieces, cut to surround a clicky 12mm square button in a sort of stepped pyramid.  The bottom piece of foam stuck very well to the helmet surface, and foam above that which didn't stick as well to the foam below got a bead of hot glue around the edge.  They're plenty water-proof since I hot glued any place water could get in.  A small Case Logic hearing aid case attached to the goggle strap on the rear of the helmet holds the electronics-- bluetooth board, connections, battery and charger circuit; appropriate since it's a sort of hearing aid image

     

    The project is complete and the helmet has had two glorious, rocking days out on the slopes.  It works just like I'd hoped, giving me full remote control of my iPhone with gloved hands while flying down the mountain.  I got plenty of funny looks and people asking "what's up with your  helmet?"

     

    I'll post pictures and a demo video soon, thanks for the replies!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jmsaltzman
    0 jmsaltzman over 15 years ago

    I came up with a good solution using a stack of adhesive-backed craft foam pieces, cut to surround a clicky 12mm square button in a sort of stepped pyramid.  The bottom piece of foam stuck very well to the helmet surface, and foam above that which didn't stick as well to the foam below got a bead of hot glue around the edge.  They're plenty water-proof since I hot glued any place water could get in.  A small Case Logic hearing aid case attached to the goggle strap on the rear of the helmet holds the electronics-- bluetooth board, connections, battery and charger circuit; appropriate since it's a sort of hearing aid image

     

    The project is complete and the helmet has had two glorious, rocking days out on the slopes.  It works just like I'd hoped, giving me full remote control of my iPhone with gloved hands while flying down the mountain.  I got plenty of funny looks and people asking "what's up with your  helmet?"

     

    I'll post pictures and a demo video soon, thanks for the replies!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • Catwell
    0 Catwell over 15 years ago in reply to jmsaltzman

    Jmsaltzman,

     

    Post pictures and schematics of what your final design ended up being.

     

    Looking forward to it.

     

    Cabe