Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum MyGenWashy: From Vienna Hackathon to Open Source Smart Washing Machines — A Blueprint for Resilient Tech
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 325 subscribers
  • Views 5363 views
  • Users 0 members are here
  • washing machine
  • recycle
  • hackathon
  • open source
  • electronics
  • digital product pass
  • open source hardware
Related

MyGenWashy: From Vienna Hackathon to Open Source Smart Washing Machines — A Blueprint for Resilient Tech

mayermakes
mayermakes over 1 year ago

It all started at Mariahilfer i, Vienna’s grassroots hub for resilient technologies, circular economy
projects, and hacking culture. During a hackathon hosted in this unique space—also home to the
Kintsugi Repair Café—Patrick Awart of IoT Austria kicked off an ambitious idea: Give old,
mechanically sound washing machines a second life by retrofitting them with open-source, smart
control electronics.

The project immediately resonated with Clemens Mayer—known to many in the Element14
Community simply as Clem. Clem is well known for his personal mission to ensure there’s at least
one reliable, open-source version of every essential technology, strengthening society’s resilience in
the face of closed ecosystems and throwaway culture. So naturally, he jumped on board.

Backed by Mayer Makes, IoT Austria, and the Mariahilfer i community, the MyGenWashy project
quickly evolved beyond a weekend hack—blending hardware hacking, Smart Home integration,
repair culture, and open-source compliance into one focused initiative.

Smart Tech Meets Circular Economy

MyGenWashy retrofits old washing machines with generic control boards, designed to integrate
seamlessly into Smart Home systems via ESPHome and Home Assistant. Thanks to IoT Austria's
early ESPHome integration efforts, the machines can already be monitored and controlled over
local networks — with future interface options including reusing old smartphones as intuitive
displays and touch controls.
From a technical perspective, the team uncovered fascinating aspects of washing machine design
during teardown and reverse-engineering:

  • Air Pressure Water Level Control: A refreshingly simple mechanical system regulates
    water levels—efficient and reliable.
  • Mechanical Safety First: Even generic control boards include hardware-based protections
    against overflow and overheating.
  • Simplicity at Scale: Many washing machines, regardless of price point, share common
    components like Darlington ULN2003 relay drivers.

The takeaway? The hardware is already durable. By replacing only the electronics with open, user-
serviceable, and Smart Home-compatible alternatives, we extend appliance life, cut electronic
waste, and empower users.

The Power of Community and Open Source Certification

This project isn't happening in isolation. Mariahilfer i also hosts the Kintsugi Repair Café, making
it the perfect hacking ground for repair-focused experimentation.
MyGenWashy ties directly into Smander.com's work on the Open Digital Product Pass (ODPP) —
an ambitious initiative to fulfill upcoming EU requirements for product transparency, circular
economy documentation, and CE-compliant, truly open-source hardware. In partnership withregulatory experts, ODPP aims to create verifiable, safe open-source designs that meet real-world
legal and technical standards.

image

image

Generous Hardware Support for a Repairable Future

The project wouldn’t have accelerated this fast without crucial support from hardware allies:

  • AISLER generously provided professional-quality PCBs for the prototype and development
    phases, reinforcing their commitment to local, small-batch, repair-friendly production.

  • Farnell contributed essential components, helping Makers and engineers realize a fully
    functional control board with energy-efficient, Smart Home-ready capabilities.

This shared mission—making hardware repairable, modifiable, and accessible—is at the heart of
the broader movement MyGenWashy embodies.

Once we get to a stage where Certification comes into play we can count on Smander.com to achieve this milestone.

Open Source, Fully Documented, Ready to Evolve

The complete MyGenWashy design, including schematics, component lists, and ESPHome
configurations, is available on GitHub for replication, modification, and iteration:
https://github.com/mayermakes/MyGenWashy
Beyond washing machines, the principles apply to other household devices—building a blueprint
for modular, repairable, connected hardware with community-driven innovation at its core.

Join the Mission: One Open Source Version of Everything

For Clem, Patrick Awart, Thomas Losert, and the wider community, this is more than a project—it’s
a movement toward resilient, sustainable technology.

  • Want to contribute to ODPP, open hardware standards, or MyGenWashy v2 and v3?
  • Interested in creating open-source, compliant alternatives to everyday tech?
  • Believe in empowering users to repair, reuse, and innovate?

The door is open:

contribute@odpp.at

http://odpp.at

Together, we can ensure the technology we rely on remains transparent, repairable, and open—
because resilient societies are built on resilient tools.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 1 year ago +5
    Hi, I've not looked in detail, but one thing that would really bug me, is that there's live mains just an accidental touch away, on that TO-220 triac sticking up, likely taller than any other part too…
  • DAB
    DAB over 1 year ago +3
    I like the idea. Us older folk just want a simple device that is easy to use and does a good job.
  • Robert Peter Oakes
    Robert Peter Oakes over 1 year ago +2
    Awesome project, At a minimum it is a great way to introduce people to how commercial / consumer appliances are designed (Good and Bad :) I would think the same principles could also be applied to AC Home…
Parents
  • michaelkellett
    michaelkellett over 1 year ago

    I had a look at as much of this as I could find.

    I'm baffled - there is talk of documentation - but where is it ?

    There is a Github project for the pcb and some parts lists, a very, very top level presentation and ......

    Where is the specification, the architecture description (software and hardware), some discussion about how washing machines work (and which subset is targeted by this project) etc.etc.

    I'd expect to see some analysis of the efficiency of the washing machines (massively improved over the last 20 years) and how the Open Source Controller might contribute to that - or not.

    I could get quite interested in this project (our own LG machine is getting on - about 12 years old and its rotary control is getting a little quirky) but I don't seem to able to find my way in.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 1 year ago in reply to michaelkellett

    Thanks for the interest!

    the documentation is right on the github https://github.com/mayermakes/MyGenWashy
    The PCB is just the first outcome of the Hackathon, we are currently waiting on the pCb and PArts to build it up. Then write its firmware and integrate it into our test machine. 
    Washingmachines have not changed at all at their core in the last 20 years the only thing that we found different in the various models we looked at are the control and User interface sections, but topological they were all pretty much the same. Our Control board hooks into these commone components and takes care of the basic functions like motor control, relays etc. and connects via I2C to the UI side which can be whatever you want( from. a simple tactile Knob and buttons, or ESP32 that hooks into your network and displays the UI on a phone).Architectural this is the central control unit that all washing machines have but open source and using generic  easily substituteable components.

    The Safety interlock system is directly implemented in Hardware. The Relay logic is active as soon as the unit is powered and does not need the MCU at all to function. This includes door, heater and Water level Sensors. You can see it all within the schematic.

    In essence Washing machines of current design, are topological : 2 Valves, a pump, an AC motor, Heater and the safety interlock system (I consider the Water level sensor part of it). 
    Then there is a machine control and a UI powered by MCUs. we found soem machines use just a single MCU for both tasks, and utilize highly specialized ICs for tasks like motor control.
    We decided to avoid any hard to source or even proprietary components, so we use a ATtiny3226 (replaceable with almost any other mcu in practice) strictly for control and a separate MCu for UI with strictly separated tasks. These are connected via an I2C bus that allows simple integration of more additional sensors.

    Most efficiency gains seem to stem not from big technical changes but from better washing detergents that work sufficiently at lower temperatures and deliberate conservation of energy through washing programs that more targeted use heating, rinsing and tumbling cycles and are tailored to modern washing detergents.
    We see almost all changes on the UI side while the actual working principle stayed the same and is already very robust, safe  and efficient.

    There is no guarantee someone could come up with an even more efficient washing program than is already established, but in case a machine is broken, the most likely part to break could be replaced with a repairable open solution and keep the machine in ciculation. 
    I'm personally interested most in the aspect of tailoring the User interface to my personal preferences,
    so I don´t need to click through touch menus or confusing buttons and could implement an "even Clem can wash now" system that just has simple "underwear", "Work clothes" & "other" buttons.

    So of course there no super extensive Documentation yet as we just started with our hackathon.
    V1 pcb will be integrated into the machine in the pictures and used for Firmware Development.(that is why its tht so we can make easy bodges and probe all contacts from the back.)
    V2 will implement any changes /fixes and move to mostly smd assembly for better component availability.
    V3 will then start the roadmap towards certification and sealing for a unit that could actually be deployed.

    So I would have loved to just link documentation for V3 but we are not there yet. ;-)


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 1 year ago in reply to mayermakes

    Hello Clem,

    Thanks for the additional info.

    I think maybe you are starting from a somewhat wrong assumption:

    Washingmachines have not changed at all at their core in the last 20 years the only thing that we found different in the various models we looked at are the control and User interface sections, but topological they were all pretty much the same

    I Googled (actually DuckDuckgoed)

    "how many washing machines use direct drive motors"

    Which will give you lots of useful information, although I didn't get the answer to my question.

    https://faq-washer.com/direct-drive-washing-machines/

    There are also inverter drive machines.

    It's interesting that LG offer a 10 year warranty on their direct drive machines which also do clever stuff like load balancing and weighing by precision control of the drum rotation and measuring the motor current. This enables them to tune the washing time according to the load (and still get the delayed time right   - it times to the end of the cycle and the cycle can vary by 2:1 in length).

    But I don't know what proportion of machines use direct drive.

    OK, I understand that you are right at the start of the project -  but in the areas I've worked in documentation comes first (not all of it of course) - it does help avoid a great many issues.

    The following is offered in a spirit of helpfulness although you might not like reading it much:

    I've been looking at your PCB and I'm worried that you don't have the clearances you need for 230V AC (nominal) working in a damp environment. There is a lot of stuff on the web about PCB clearances and what's required for different voltages, environments and positions in the system.

    The consensus would be that you need 2mm minimum for 230VAC unless failure will expose the operator to the dangerous voltage in which case you need a lot more. Some regulations if different places make very specific demands which must be met.

    You've got 0.2mm clearance in several places on the board - (eg MOTOR_230_LIVE to Q1 gate) and many instances of less than 2mm separation. The 0.2mm clearances are so small that trouble is pretty much a certainty. Some of the larger clearances are not safe but might be acceptable if the whole board is isolated, but I can't tell if it is.

    (BTW, this stuff really matters, a long time ago where I was working we had a lapping machine with a mains powered controller with mains and control stuff on the same PCB, and not enough clearance. The PCB was coated, but not well enough and every few months would get damp, develop a conductive path from mains to something, get hot, char the board, set the board on fire and then we would see the magic smoke coming out of the box. And fit a new board which we kept in stock.)

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 1 year ago in reply to mayermakes

    Hello Clem,

    Thanks for the additional info.

    I think maybe you are starting from a somewhat wrong assumption:

    Washingmachines have not changed at all at their core in the last 20 years the only thing that we found different in the various models we looked at are the control and User interface sections, but topological they were all pretty much the same

    I Googled (actually DuckDuckgoed)

    "how many washing machines use direct drive motors"

    Which will give you lots of useful information, although I didn't get the answer to my question.

    https://faq-washer.com/direct-drive-washing-machines/

    There are also inverter drive machines.

    It's interesting that LG offer a 10 year warranty on their direct drive machines which also do clever stuff like load balancing and weighing by precision control of the drum rotation and measuring the motor current. This enables them to tune the washing time according to the load (and still get the delayed time right   - it times to the end of the cycle and the cycle can vary by 2:1 in length).

    But I don't know what proportion of machines use direct drive.

    OK, I understand that you are right at the start of the project -  but in the areas I've worked in documentation comes first (not all of it of course) - it does help avoid a great many issues.

    The following is offered in a spirit of helpfulness although you might not like reading it much:

    I've been looking at your PCB and I'm worried that you don't have the clearances you need for 230V AC (nominal) working in a damp environment. There is a lot of stuff on the web about PCB clearances and what's required for different voltages, environments and positions in the system.

    The consensus would be that you need 2mm minimum for 230VAC unless failure will expose the operator to the dangerous voltage in which case you need a lot more. Some regulations if different places make very specific demands which must be met.

    You've got 0.2mm clearance in several places on the board - (eg MOTOR_230_LIVE to Q1 gate) and many instances of less than 2mm separation. The 0.2mm clearances are so small that trouble is pretty much a certainty. Some of the larger clearances are not safe but might be acceptable if the whole board is isolated, but I can't tell if it is.

    (BTW, this stuff really matters, a long time ago where I was working we had a lapping machine with a mains powered controller with mains and control stuff on the same PCB, and not enough clearance. The PCB was coated, but not well enough and every few months would get damp, develop a conductive path from mains to something, get hot, char the board, set the board on fire and then we would see the magic smoke coming out of the box. And fit a new board which we kept in stock.)

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mayermakes
    mayermakes over 1 year ago in reply to michaelkellett

    I especially like to read critique!

    Good point on the clearance. since the goal was to verify operation assumptions with V1 (and routing had to be done within a few hours) i just left approximate spaces, and mainly aimed to fit it within a space that wont make the pcb to expensive (its also only 2 layer) . In operation the whole board would be coated/covered for water tightness.
    but we won´t do that step until V3.
    For V2 I intend to put all 230V sections on its own board, just coupled via optoisolators which should also allow to tuck it into more models of washing machines with tighter spaces on the inside. and possibly easier access for repairs.

    since we focused on getting broken machines back into operation, direct drive and other rather niche Variants were not in scope. So we basicalyl looked at the most common scenario: a  medium segment machine from the last 10-15 years breaks down-> get it back working.

    the inclusion of the i2c bus is our route to include these newer niche features down the line, as it requires additional sensors.

    In the area I come from we need to get stuff working first (somehow) and then we make it pretty. Once the pretty stage starts we can spend more time on documentation.
    Since the project is open for more people to join , I would hope for a documentation enthusiast to take over that part as  such a person would certainly do a great job at it!