Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum BeagleBoard-X15: new OSHW from BeagleBoard.org
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 328 subscribers
  • Views 1990 views
  • Users 0 members are here
  • open_source
  • oshw
  • pru
  • embedded
  • dsp
  • open_hardware
  • beagleboard
  • linux
Related

BeagleBoard-X15: new OSHW from BeagleBoard.org

fustini
fustini over 11 years ago

Official announcement today from jkridner & BeagleBoard.org:

 

image

BeagleBoard.org - 2015-10-14-beagleboard-x15

Announcing the new powerful BeagleBoard-X15 open hardware computer for electronics innovators from BeagleBoard.org

Innovate with an open community of developers on the most powerful and flexible open hardware computer development system available

 

 

 

 

 

Powered by a SitaraTm AM572x processor from Texas Instruments (TI) [...] dual ARMRegistered CortexRegistered-A15 cores clocked at 1.5GHz [...] Accelerated processing of physical world data is made easier than ever with the dual C66x digital signal processors (DSPs) supported by OpenCL

 

 

There is a form to register your interest in BeagleBoard-X15 for delivery in time for Christmas:


http://beagleboard.org/X15

 

 

Here the wiki page with more details:

 

Beagleboard:BeagleBoard-X15 - eLinux.org

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 11 years ago +2
    David Scheltema ( interested1 has written a great post about BeagleBoard-X15 on MAKE Blog BeagleBoard Officially Reveals the X15 — And it’s a Beast http://makezine.com/2015/10/14/beagleboard-officially…
  • johnbeetem
    johnbeetem over 11 years ago +2
    I'll be interested to see how it performs compared to the US$74 ODROID-XU4, which has quad 2 GHz Cortex-A15 and quad 1.4 GHz Cortex-A7. For real-time applications, the PRU, DSP, and Cortex-M4 are very…
  • johnbeetem
    johnbeetem over 11 years ago in reply to shabaz +2
    shabaz wrote: No idea on throughput capability, but given it is 128-bit wide and non-blocking according to a deepchip post it could be a spectacular amount of throughput between modules simultaneously…
Parents
  • shabaz
    shabaz over 11 years ago

    Hi Drew,

     

    Thanks for the links!

    Really looking forward to this at Christmas (apart from Christmas itself, and Star Wars. Speaking of which, great that the BeagleBone color scheme is still black!).

    This board looks like in reality it may have at least an order of magnitude greater realistically-usable performance than its predecessor, due to the addition of the multiple Cortex-M, DSP and GPU cores.

    And love the high-speed interfaces that provide perhaps a hundred-fold increase in I/O throughput with GigEth and USB 3.0 on the board. So much to look forward to.

     

    Here is a tidied-up diagram of the processor that we can use for blogs/annotations perhaps.

    (It is the same as the one in the TRM, but removed of the color so we can highlight bits of it with the black-and-white one, since there will be a lot of topics to discuss, and the other

    one with more color where orange is video related, red is processing power, etc).

    I'll place colored and black-and-white PNG and SVG format files in the BeagleBone section tomorrow and on elinux.

     

    image

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 11 years ago

    Hi Drew,

     

    Thanks for the links!

    Really looking forward to this at Christmas (apart from Christmas itself, and Star Wars. Speaking of which, great that the BeagleBone color scheme is still black!).

    This board looks like in reality it may have at least an order of magnitude greater realistically-usable performance than its predecessor, due to the addition of the multiple Cortex-M, DSP and GPU cores.

    And love the high-speed interfaces that provide perhaps a hundred-fold increase in I/O throughput with GigEth and USB 3.0 on the board. So much to look forward to.

     

    Here is a tidied-up diagram of the processor that we can use for blogs/annotations perhaps.

    (It is the same as the one in the TRM, but removed of the color so we can highlight bits of it with the black-and-white one, since there will be a lot of topics to discuss, and the other

    one with more color where orange is video related, red is processing power, etc).

    I'll place colored and black-and-white PNG and SVG format files in the BeagleBone section tomorrow and on elinux.