Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum BeagleBoard-X15: new OSHW from BeagleBoard.org
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 328 subscribers
  • Views 1990 views
  • Users 0 members are here
  • open_source
  • oshw
  • pru
  • embedded
  • dsp
  • open_hardware
  • beagleboard
  • linux
Related

BeagleBoard-X15: new OSHW from BeagleBoard.org

fustini
fustini over 11 years ago

Official announcement today from jkridner & BeagleBoard.org:

 

image

BeagleBoard.org - 2015-10-14-beagleboard-x15

Announcing the new powerful BeagleBoard-X15 open hardware computer for electronics innovators from BeagleBoard.org

Innovate with an open community of developers on the most powerful and flexible open hardware computer development system available

 

 

 

 

 

Powered by a SitaraTm AM572x processor from Texas Instruments (TI) [...] dual ARMRegistered CortexRegistered-A15 cores clocked at 1.5GHz [...] Accelerated processing of physical world data is made easier than ever with the dual C66x digital signal processors (DSPs) supported by OpenCL

 

 

There is a form to register your interest in BeagleBoard-X15 for delivery in time for Christmas:


http://beagleboard.org/X15

 

 

Here the wiki page with more details:

 

Beagleboard:BeagleBoard-X15 - eLinux.org

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 11 years ago +2
    David Scheltema ( interested1 has written a great post about BeagleBoard-X15 on MAKE Blog BeagleBoard Officially Reveals the X15 — And it’s a Beast http://makezine.com/2015/10/14/beagleboard-officially…
  • johnbeetem
    johnbeetem over 11 years ago +2
    I'll be interested to see how it performs compared to the US$74 ODROID-XU4, which has quad 2 GHz Cortex-A15 and quad 1.4 GHz Cortex-A7. For real-time applications, the PRU, DSP, and Cortex-M4 are very…
  • johnbeetem
    johnbeetem over 11 years ago in reply to shabaz +2
    shabaz wrote: No idea on throughput capability, but given it is 128-bit wide and non-blocking according to a deepchip post it could be a spectacular amount of throughput between modules simultaneously…
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    I'll be interested to see how it performs compared to the US$74 ODROID-XU4, which has quad 2 GHz Cortex-A15 and quad 1.4 GHz Cortex-A7.  For real-time applications, the PRU, DSP, and Cortex-M4 are very attractive.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 11 years ago in reply to johnbeetem

    Yeah, I think there are other boards that provide a better value in terms of application processor performance to run Linux.  I agree the combination of all those on-die processors will make X15 appealing for real-time systems.

     

    This discussion also came up on the beagleboard mailing list:

    https://groups.google.com/forum/#!category-topic/beagleboard/_PfeLrGSEKI

     

    I had asked if people knew of other suppliers that include a microcontroller on-die with a Cortex-A series processor.  One person pointed out the Xilinix Zynq combines a "hard" Cortex-A processor with a FPGA.  Someone else wrote that the Freescale i.MX6 is going to have a Cortex-M4 on-die.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 10 years ago in reply to fustini

    The UDOO Neo uses an i.MX 6SoloX processor that has a 1 GHz Cortex A9 and a 200 MHz Cortex M4 core in it.  It has dual row Arduino compatible (3.3V I/0) connectors

    with software that dedicates one row of those pins to the M4 core with the other row of pins dedicated to the A9 core. It also has a Arduino compatible IDE for the M4 core

    with the A9 running Linux of course.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 10 years ago in reply to fustini

    The UDOO Neo uses an i.MX 6SoloX processor that has a 1 GHz Cortex A9 and a 200 MHz Cortex M4 core in it.  It has dual row Arduino compatible (3.3V I/0) connectors

    with software that dedicates one row of those pins to the M4 core with the other row of pins dedicated to the A9 core. It also has a Arduino compatible IDE for the M4 core

    with the A9 running Linux of course.