Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum BeagleBoard-X15: new OSHW from BeagleBoard.org
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 328 subscribers
  • Views 1997 views
  • Users 0 members are here
  • open_source
  • oshw
  • pru
  • embedded
  • dsp
  • open_hardware
  • beagleboard
  • linux
Related

BeagleBoard-X15: new OSHW from BeagleBoard.org

fustini
fustini over 11 years ago

Official announcement today from jkridner & BeagleBoard.org:

 

image

BeagleBoard.org - 2015-10-14-beagleboard-x15

Announcing the new powerful BeagleBoard-X15 open hardware computer for electronics innovators from BeagleBoard.org

Innovate with an open community of developers on the most powerful and flexible open hardware computer development system available

 

 

 

 

 

Powered by a SitaraTm AM572x processor from Texas Instruments (TI) [...] dual ARMRegistered CortexRegistered-A15 cores clocked at 1.5GHz [...] Accelerated processing of physical world data is made easier than ever with the dual C66x digital signal processors (DSPs) supported by OpenCL

 

 

There is a form to register your interest in BeagleBoard-X15 for delivery in time for Christmas:


http://beagleboard.org/X15

 

 

Here the wiki page with more details:

 

Beagleboard:BeagleBoard-X15 - eLinux.org

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 11 years ago +2
    David Scheltema ( interested1 has written a great post about BeagleBoard-X15 on MAKE Blog BeagleBoard Officially Reveals the X15 — And it’s a Beast http://makezine.com/2015/10/14/beagleboard-officially…
  • johnbeetem
    johnbeetem over 11 years ago +2
    I'll be interested to see how it performs compared to the US$74 ODROID-XU4, which has quad 2 GHz Cortex-A15 and quad 1.4 GHz Cortex-A7. For real-time applications, the PRU, DSP, and Cortex-M4 are very…
  • johnbeetem
    johnbeetem over 11 years ago in reply to shabaz +2
    shabaz wrote: No idea on throughput capability, but given it is 128-bit wide and non-blocking according to a deepchip post it could be a spectacular amount of throughput between modules simultaneously…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    It looks like an interesting motherboard.  The eSATA connector and GHz Ethernet capability is definitely welcome for high-speed local storage and networking respectively.

     

    I have to agree with johnbeetem that at USD 239.00, this seems to be a high price tag considering the competition in desktop and server motherboard markets.  Also:

    • At 4" x 4.2" (unique form factor), there is no existing off-the-shelf protective enclosure available.  Their customer base probably can eventually produce 3D-print STL files for enclosures.
    • Cooling heat-sinks and fans should be an interesting adventure too.  Again, the customer base should rise to the occasion, given the investment.
    • For RAM, you get exactly 2GB DDR3L at 533 MHz (~8,500 MB/sec max).  "Beast"?  Most moderately-priced DDR3/3L packages sold nowadays are DDR3-1333 (10,666 MB/sec max) or DDR3-1600 (12,800 MB/sec max).
    • Why should a customer incur the cost of a second 1GHz RJ-45 connector?  Maybe, they are thinking about network infrastructure applications where physical separation on this board is desirable (E.g. router or proxy)?

     

    clem57 - if you buy one of these, I would love to come over and see it!  Any other perspective buyers live in the DFW Texas area?  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    It looks like an interesting motherboard.  The eSATA connector and GHz Ethernet capability is definitely welcome for high-speed local storage and networking respectively.

     

    I have to agree with johnbeetem that at USD 239.00, this seems to be a high price tag considering the competition in desktop and server motherboard markets.  Also:

    • At 4" x 4.2" (unique form factor), there is no existing off-the-shelf protective enclosure available.  Their customer base probably can eventually produce 3D-print STL files for enclosures.
    • Cooling heat-sinks and fans should be an interesting adventure too.  Again, the customer base should rise to the occasion, given the investment.
    • For RAM, you get exactly 2GB DDR3L at 533 MHz (~8,500 MB/sec max).  "Beast"?  Most moderately-priced DDR3/3L packages sold nowadays are DDR3-1333 (10,666 MB/sec max) or DDR3-1600 (12,800 MB/sec max).
    • Why should a customer incur the cost of a second 1GHz RJ-45 connector?  Maybe, they are thinking about network infrastructure applications where physical separation on this board is desirable (E.g. router or proxy)?

     

    clem57 - if you buy one of these, I would love to come over and see it!  Any other perspective buyers live in the DFW Texas area?  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    I still have a Pine 64 coming to play with. I will have to put my spending in check for now. image

    Clem