Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Polls Are any SBCs ready to replace desktop computers?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: johnbeetem
  • Date Created: 16 Nov 2014 11:51 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:01 PM
  • Views 5980 views
  • Likes 1 like
  • Comments 27 comments
Related
Recommended

Are any SBCs ready to replace desktop computers?

I would love to replace my power-hungry desktop PC with an inexpensive SBC with no audible fan.  However, so far the SBCs I've tried lately (BeagleBone, Raspberry Pi, BeagleBoard) don't have enough processing power to be a viable desktop PC.

 

So, are any of the higher-performance SBCs that have been released lately up to the task?  I'm looking for a GNU/Linux computer that can do a decent job surfing the Internet (I don't care about video or audio performance) and a decent job compiling C programs.  I would say it needs at least 1 GB RAM and SATA for a disk drive.  100 Mb/s Ethernet is adequate, but I'd prefer not going through a USB hub.  Reasonable number of USB ports and HDMI output.  Wi-Fi is not needed or desired.

 

Here are some of the SBCs I've been watching and might consider.  Feel free to add others!  Most of these are OSHW, which is of course preferred.

 

Banana Pi: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

CubieTruck: Allwinner A20 Dual ARM Cortex-A7, 2 GB DDR3, SATA, GBE.

Intel Next Unit of Computing (NUC): Intel Atom or other, up to 8 GB DDR3, SATA, GBE.

MinnowBoard MAX: Intel Atom, 1 or 2 GB DDR3, SATA, GBE.

Olimex LIME2: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

PCduino3Nano: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

RIoTboard: Freescale i.MX6 ARM Cortex-A9, 1GB DDR3, no SATA, GBE.

Wandboard Quad: Freescale i.MX6 Quad ARM Cortex-A9, 2 GB DDR3, SATA, GBE.

  • sbc
  • oshw
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 11 years ago +5
    Hi John! I've not used many of these, so I can't comment with much knowledge, but I suspect RIoTboard is getting there, certainly running Android it is speedy (if one is happy running Android to do work…
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild +3
    A nice pic of my XU on the back of one of my monitors.
  • fustini
    fustini over 11 years ago in reply to fustini +3
    johnbeetem - I've been using the MinnowBoard MAX as my 3-D printing workstation and love it! I have a USB 3.0 memory stick for the main disk running Ubuntu. It is really the first time I've used a single…
  • Problemchild
    Problemchild over 11 years ago in reply to johnbeetem

    Indeed crazy to think with the 128GB micro sd card in my phone I now have 160GB on a phone ... just need a hover car now

     

    BTW saw some one's phone case that a company had put a picture of her cat on ..cute stuff sells!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to Problemchild

    John Alexander wrote:

     

    Nice Video John, The box was rather stylish too, rather fun and non computer looking so a good choice in my mind.

    What did you use the 'bone for in that box?

    That's a BeagleBoard B4 with 128MB DRAM, bought in July 2008 before the mad rush.  It was my first ARM development board, and I still use it as a test target for XXICC (http://www.element14.com/community/groups/fpga-group/blog/2014/11/15/xxicc-21st-century-co-design-release-00m).  I had hoped that it would have been a suitable "main machine", but with only 128MB and no SATA that's really not possible.  Browsers are such resource hogs, and I like to be able to check e-mail and web sites without having to switch machines.  BeagleBoard does fine running my code since my programming ethos was formed in the punch card era when carrying around more than 4 KLOC was impractical image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to najath

    Check out my video earlier in the thread full 1080p isn't a problem for it at all and it's even better now.

    There's even XBMC on the menu system if you like that kind of thing image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to johnbeetem

    Nice Video John, The box was rater stylish too, rather fun and non computer looking so a good choice in my mind.

    What did you use the 'bone for in that box?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • najath
    najath over 11 years ago

    recently tried an Intel NUC with atom processor (E3815). Its like a minnowBoard inside a nice casing - same processor, etc. But as fustini mentioned, there are no GPIO to play with. It is more like a final product than a board to play around with.

     

    Performance reminds me of the first PC I had, that ran windows XP. Now I'm using it to run xbmc on top of Tizen. The only draw back I saw was after some time there is lag between the audio and video. Not sure whether it has something to do with not properly setting up the system. I have not tried a conventional Linux distro on it yet. Thinking of buying a sata drive, to explore its full capability.

     

    I also have a sabrelite board, which is similar to wandboard Quad. I had tried Ubuntu Trusty LXDE version on it. The browser is a bit slow. The problem could be due to running from SD Card. SSD should give a better performance, but have not tried that yet

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to Problemchild

    John Alexander wrote:

     

    We could do one but really prefer someone else to do the design

     

    Well, there's always the candy box method...

     

    https://www.youtube.com/watch?feature=player_embedded&v=Jf9sTx3pElk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to johnbeetem

    We could do one but really prefer someone else to do the design

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago

    Woo-hoo!  Someone voted for PCduino3Nano!  I'd love to hear further comments.  That seems like an amazingly powerful board for US$40.  I wonder if someone offers a case with space for a 2.5" SATA hard disk?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 11 years ago in reply to johnbeetem

    Hi, Roma was excellent.  And the videos of the Open Hadware Summit are now online:

    Open Hardware Summit 2014 - Rome on Vimeo

     

    I also did a presentation at my hackerspace [PDF on Google Drive]:

    https://docs.google.com/file/d/0B_NI2VDamOOfVWlBd0dwT0VweFE/view

     

    re: minnowboard max, I actually let an embedded developer at my hackerspace borrow it until he gets his.  He is very excited as Android Open Source Platform (AOSP) has a build target for the MinnowBoard MAX.  He said there is no other board that he can use to get a head start on the new Intel "Baytrail" Atom-based system his company is developing (in-flight entertainment system).

     

    re: ISE, I will definitely try that out when I get it back to see how painful synthesize is.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to Problemchild

    John Alexander wrote:

     

    This certainly be interesting for an application where you need INTEL CPU compatibility for the application.

    ISE is a good example there: are so many commercial apps you would never get an ARM binary for in a million years.

    IIRC, in the early years of Xilinx their software only ran on "workstations", typically 680x0 or SPARC.  PC was added later, and initially could only be used for very small Xilinx devices.

     

    As soon as 64-bit ARMs take over desktops and laptops, you'll see Xilinx and many others support them.  For Xilinx it's easy, since its software has run on Unix since the early years.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>