Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Polls Are any SBCs ready to replace desktop computers?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: johnbeetem
  • Date Created: 16 Nov 2014 11:51 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:01 PM
  • Views 5986 views
  • Likes 1 like
  • Comments 27 comments
Related
Recommended

Are any SBCs ready to replace desktop computers?

I would love to replace my power-hungry desktop PC with an inexpensive SBC with no audible fan.  However, so far the SBCs I've tried lately (BeagleBone, Raspberry Pi, BeagleBoard) don't have enough processing power to be a viable desktop PC.

 

So, are any of the higher-performance SBCs that have been released lately up to the task?  I'm looking for a GNU/Linux computer that can do a decent job surfing the Internet (I don't care about video or audio performance) and a decent job compiling C programs.  I would say it needs at least 1 GB RAM and SATA for a disk drive.  100 Mb/s Ethernet is adequate, but I'd prefer not going through a USB hub.  Reasonable number of USB ports and HDMI output.  Wi-Fi is not needed or desired.

 

Here are some of the SBCs I've been watching and might consider.  Feel free to add others!  Most of these are OSHW, which is of course preferred.

 

Banana Pi: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

CubieTruck: Allwinner A20 Dual ARM Cortex-A7, 2 GB DDR3, SATA, GBE.

Intel Next Unit of Computing (NUC): Intel Atom or other, up to 8 GB DDR3, SATA, GBE.

MinnowBoard MAX: Intel Atom, 1 or 2 GB DDR3, SATA, GBE.

Olimex LIME2: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

PCduino3Nano: Allwinner A20 Dual ARM Cortex-A7, 1 GB DDR3, SATA, GBE.

RIoTboard: Freescale i.MX6 ARM Cortex-A9, 1GB DDR3, no SATA, GBE.

Wandboard Quad: Freescale i.MX6 Quad ARM Cortex-A9, 2 GB DDR3, SATA, GBE.

  • sbc
  • oshw
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 11 years ago +5
    Hi John! I've not used many of these, so I can't comment with much knowledge, but I suspect RIoTboard is getting there, certainly running Android it is speedy (if one is happy running Android to do work…
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild +3
    A nice pic of my XU on the back of one of my monitors.
  • fustini
    fustini over 11 years ago in reply to fustini +3
    johnbeetem - I've been using the MinnowBoard MAX as my 3-D printing workstation and love it! I have a USB 3.0 memory stick for the main disk running Ubuntu. It is really the first time I've used a single…
  • Problemchild
    Problemchild over 11 years ago in reply to johnbeetem

    This certainly be interesting for an application where you need INTEL CPU compatibility for the application.

    ISE is a good example there are so many commercial apps you would never get an ARM  binary for in a million years.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to fustini

    Drew Fustini wrote:

     

    Interesting poll!

     

    I recently got a MinnowBoard MAX so I've been playing around with it: https://gist.github.com/pdp7/e1e54f6c77f76f198564

     

    I think it has more power than any of the ARM boards listed though I've not done any benchmarks yet.

     

    ...

     

    The WandBoard with the Freescale Quad i.MX6 I think would be a good balance of power efficiency and processing power.  Bunnie selected it for his Open Source Hardware laptop, the Novena: https://www.crowdsupply.com/kosagi/novena-open-laptop

     

    ...at least I hope so since I ordered one.  I should be able to comment in early 2015 on how much I like it.

    Hi Drew, it's good to hear from you.  How was Roma?

     

    I'll be interested in your impression of MinnowBoard MAX after you've played with it for a while.  I saw and touched one at the 2014 ESC AKA "EE Live!" earlier this year and I was impressed by how cool it ran, especially compared to an Intel Galileo.  With 2GB it might be able to run Xilinx ISE -- I wonder how well?

     

    I'll also be interested in Novena reviews when users get their hands on them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild

    And a video of the U3 which is the affordable quadcore...nice

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild

    A nice pic of my XU on the back of one of my monitors.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    yes Shabaz I have some of those available too! image

     

    Not fast enough then you can get the XU or XU3 thunderbolts and lightning image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 11 years ago

    Interesting poll!

     

    I recently got a MinnowBoard MAX so I've been playing around with it: https://gist.github.com/pdp7/e1e54f6c77f76f198564

     

    I think it has more power than any of the ARM boards listed though I've not done any benchmarks yet.

     

    However, I think ARM boards generally do better a power consumption (though opinions differ whether I'm talking to Intel or ARM-based vendors at conferences ).

     

    The WandBoard with the Freescale Quad i.MX6 I think would be a good balance of power effiency and processing power.  Bunnie selected it for his Open Source Hardware laptop, the Novena: https://www.crowdsupply.com/kosagi/novena-open-laptop

     

    ...at least I hope so since I ordered one    I should be able to comment in early 2015 on how much I like it.

     

    BTW, I would probably list Intel NUC as number #1 performer on the list here given that it can have 8GB RAM.  However, I don't feel it is necessarily a SBC.  Though that might just be personal bias as it doesn't have GPIO pins to play with   

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago

    Hi John!

     

    I've not used many of these, so I can't comment with much knowledge, but I suspect RIoTboard is getting there, certainly running Android it is speedy (if one is happy running Android to do work - I saw some recent post on theregister.co.uk where someone tried to run their business exclusively from a mobile phone all week - turns out they were quite successful!). I've not tried Linux on it.

    The Odroid-U3 is almost definitely a near-laptop replacement, I got very good performance running a desktop with Linux, and compiles were fast too. However it does have a heatsink! But no fan.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
<