Passive Components
  • Technologies
  • More
Passive Components
Blog Capacitor Leakage Experiments
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 19 Jul 2019 10:36 AM Date Created
  • Views 6241 views
  • Likes 12 likes
  • Comments 18 comments
  • mlcc
  • capacitors
  • experimenting
  • analog design
  • electrolytic capacitors
  • passive components
  • jc2048
  • leakage
Related
Recommended

Capacitor Leakage Experiments

jc2048
jc2048
19 Jul 2019

Introduction

 

I'm having a bit of fun experimenting. With capacitor leakage. It's all a bit ad hoc and Heath Robinson-

ish, and I'm probably setting a very bad example of how to go about engineering, but never mind. As long

as you just read it out of interest and keep saying to yourself 'why doesn't he do it properly?' or

'that's a useless way to do things, I can think of a much better way', we'll be fine. I'm doing this with

fairly minimal test equipment - just a fairly average 200MHz 'scope (a Tektronix MSO2022A) and a 5.5 digit

bench multimeter (a Fluke 8808A) - because that's all I've got; but it's always surprising what can be

done with even the simplest of gear. I'm not going to be working to great precision - the idea is to take

a qualitative look at what's going on rather than go for accurate measurements.

 

I know very little about the inner world of capacitors or, perhaps a bit more accurately given the theme

of the current blog, the various dielectrics that you'll find between the plates of capacitors. Most of

what I know is largely design advice I've picked up along the way - things like, taking into account the

bias voltage on a MLCC because of the way it reduces the capacitance, and stuff like that - without much

awareness of the actual physics involved. That means I'm not going to be teaching you anything; this is

purely exploratory and experimental.

 

The Circuit

 

The first configuration I considered was this

 

image

 

I tried building a circuit along those lines but had problems getting it stable.

 

This is the circuit configuration I went with in the end

 

 

image

 

simply pass the leakage current through a resistor and amplify the voltage difference between the ends.

 

Whatever the device is that does the amplification, it needs to have very low bias currents or the

currents into or out of the inputs will affect the reading. I don't have any instrumentation amplifiers

with those kinds of specs but I do have a LMC440 quad op amp with bias currents of only a few fA (!), so

I'm going to try making an instrumentation amplifier from that. The input offset voltage spec isn't all

that good, but for a one-off I could trim that out if it looked like being a problem.

 

For the current sense, I'm going to use a 10M resistor. That's a bit of a compromise. The value is

somewhat high for the larger possible leakage currents (up towards the uA area) and if I were doing this

again I might choose 1M and have a bit more gain on the amplifier.

 

There are various ways to make instrumentation amplifiers from op amps, but a favourite configuration is

often this one using three amplifiers

 

 

image

 

It's not too difficult to understand how it works. The output op amp is configured as a differential

amplifier. The input resistance isn't very high because of the resistors, so they are buffered by a pair

of voltage followers. Although they could literally be followers, that leads to a problem because to

change the gain would require varying two resistors at the same time in the differential amplifier.

Instead, the input pair are configured to be non-inverting with some gain [for overall unity gain, that

front-end gain can be compensated for by having a fractional gain on the differential stage]. Although

it's not immediately obvious, the lower gain setting resistors, which would normally both go to ground,

can be released from ground and simply joined together because of the symmetry of it's being a

differential amplifier, and that then leads to having one composite resistor that changes the gain of both

input amplifiers simultaneously [I'd nominate the person who thought of that for a 'Top Designer' badge,

except I don't know who it was].

 

Here's the detail of the test circuit I eventually ended up with.

 

image

 

I don't know if it was really necessary but I decided to run the whole thing off a 9V battery. That should

keep the sensitive part fairly quiet. Going for 9V allows for a reasonable range on the bias voltage and

the batteries are fairly cheap. To get a negative rail, I simply lifted the ground by three diode drops

above the battery negative. That gives me rails of about +7.2V and -1.8V on a fresh battery. Because of

that battery, it's all floating and so the arrangement won't affect connecting the output to the

oscilloscope in any way. [Note that the LMC660 can operate with a supply up to +15V. This circuit wouldn't

be safe if you were to substitute a more modern CMOS op amp designed to run on no more than 5V or 6V,

unless you were to adapt it a bit.]

 

The switch and resistor allow me to change the gain from x1 to x5. I originally intended it to be x10, but

got it wrong. (Changing the 20k to 2k by adding the 2.2k in parallel doesn't change the gain by 10, as I

thought it might.)

 

Here's the circuit as I built it on a piece of bare copper-clad board.

 

image

 

image

 

image

 

The odd arrangement with the 10k resistor, that has one end not soldered, is so that I can charge the

capacitor much more quickly than the 10M allows for. Pushing the free end down to the grounded copper

completes the circuit and the charging occurs about a thousand times quicker.

 

Here's the switched gain that I added after the other photographs were taken.

 

 

image

 

The reason that there are so many resistors around the pins of the IC socket is that I had plenty of small

1% 10k resistors, so I made the 20k ones from pairs of 10k in series.

 

The battery holder is underneath.

 

The capacitor you can see in the holder is one of the ones I was testing. It's a huge, old polystyrene

part made by winding two lengths of foil along with intermediate films of polystyrene and then heating it

so that it fuses together.

 

Doing some tests

 

When I came to try it, I immediately discovered that it would readily pick up noise, so I improvised an

electrostatic shield using a tin can from the kitchen.

 

image

 

The yellow lead connects the ground on the circuit board to the can. I did think I might need a complete

enclosure, but pushing the board back into the can was enough. Much to my delight, after I had done it I

noticed that the can, which had originally held green lentils, had "Robust and Earthy" written on the

side.

 

220nF leaded MLCC

 

First off I tried an MLCC [multi-layer ceramic capacitor] part.

 

This took a long time to settle down, but eventually the leakage ended up right down near the bottom of my

measurement range. A major problem with these measurements is that initially you are looking at the

charging currents. Then there seems to be a period where the leakage is settling down, until finally it

all levels out. Having the 10k to speed up the discharge helped, but it still took time after that.

 

image

 

This is with the gain switched to x5, so the vertical scale is equivalent to 40pA/div. Bear in mind that

this is an improvised instrumentation amplifier and the voltage offset isn't too good - it measures around

0.5mV - so this really isn't precision stuff. The temperature was about 25C (a hot summer's day for where

I am in the UK) and the bias voltage applied was set to +5V.

 

The noise on the leakage current isn't very high at all. The trace noise is very similar in level with

both the x1 and the x5 settings, so it must emanate from the amplifier, the oscilloscope, and coupled

noise rather than the capacitor.

 

At first glance, it looks like the leakage is wandering around, but there's something else going on. Have

a look at this next trace

 

image

 

That's what happens if I breathe into the tin can and suddenly change the temperature. That can't (just)

be the leakage changing because the current changes direction, so I would think it's the actual

capacitance changing, because of the dimensional changes with temperature, resulting in a discharge

current to accommodate the change. So the wandering around in the first trace is probably air currents

affecting it as I move around and not anything inherent in the leakage.

 

Here's the first trace done again with a paper tent over the whole thing to stop air moving in and out of

the can. This time the leakage current is much more steady. These thermal effects go on for a considerable

time - for this trace, I had to wait for several minutes before getting a nice steady trace after applying

the tent.

 

image

 

From that one, it looks like the final figure might be somewhere around 55pA (give or take a few tens of pA).

 

10uF 25V Electrolytic

 

This is on a gain of x1, so each division of 20mV represents 2nA. The reading of 12.8nA is higher than for

the MLCC, but is much, much better than I would have expected.

 

image

 

3.3uF 16V tantalum bead

 

Again a gain of one. This time about 200pA per division, so perhaps 160pA for the leakage. That's only

three times the MLCC figure. Again, much better than I would have expected.

 

image

 

Polystyrene

 

Here's an old polystyrene capacitor that I found. The leakage on this one was too low for me to measure

sensibly with this test setup.

 

image

 

Interestingly, the polystyrene part reacted slightly to the breathe test. As with the electrolytic, that

might well be down to dimensional changes modifying the capacitance rather than a change in the leakage,

though if so it goes in the opposite direction to the electrolytic with an immediate charge current rather

than a discharge current.

 

image

 

How does the bias voltage relate to leakage?

 

I'm going to go back to the electrolytic, as that has a reasonably high leakage that I can measure

sensibly, and try it at a few different bias voltages. There is going to be a relationship between the

voltage and the leakage current of some sort, because the potential difference is driving the current, but

does the leakage look like a simple resistance where the two are in proportion?

 

Here are the results for 1V to 5V in 1V steps. (I haven't suddenly acquired a 5-channel oscilloscope,

instead I composited the images together with Gimp.)

 

image

 

They go in order, 1V bias is the lowest and 5V bias the highest. The 5V reading is now different to what I

had yesterday (this time it's reading about 8.5pA, rather than the 12pA I got then), but this series was

taken in succession, using the same procedure each time, so should be indicative. It's quite obvious that

the relationship between voltage and leakage is very non-linear and, for an electrolytic capacitor, we

can't refer to a 'leakage resistance' in any meaningful way.

 

Just to emphasise that, here's the trace for a nominal 6V (note the change of scale). All of a sudden, the

leakage is 66n - about a thousand times what it is below 5V. [Nominal because the drop on the sense

resistor is now so high that the bias is really about 5.4V. This is now pushing against the limits of how

I've set up the circuit.]

 

image

 

All in all, it looks like an electrolytic capacitor that is operated at a fraction of its voltage rating,

this one is rated at 25V, can have a surprisingly good leakage figure at room temperature. Conversely, it

also means that to do a sensible worst-case test of the leakage probably requires a bias adjustable up to

the rated voltage.

 

This is as far as I've got at the time of first posting. I'll probably keep experimenting and, if so, I'll add any further

results as I go along.

 

If you found this interesting and would like to see more blogs I've written, a list can be found here: jc2048 Blog Index

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +6
    Hi Jon, Nice prototyping! Also the "Robust and Earthy" made me smile : ) Regarding the dual rails, I attempted using an off-the-shelf DC-DC converter visible in one of the photos here: Impact, Vibration…
  • genebren
    genebren over 7 years ago +4
    Jon, Interesting data and setup. Sure it may be a little different, but that is the cool thing about electronics, there are several ways to approach any problem. Thanks again for another deep dive with…
  • fmilburn
    fmilburn over 7 years ago +4
    Hi Jon, I really enjoyed reading this and learned a number of things. It is a delight seeing what you have done with the equipment and parts at hand. Frank
Parents
  • geralds
    geralds over 7 years ago

    Fine Project!

    What would you say, thinking about?:

    I would spend a bit more parts for the UB- Voltage splitter. I think, that the voltages may swing a bit if you connect the testing device.

    With an OPAMP it would be a bit more stabile.

    Like this schematic, the 4. OPAMP of your schematic and a few parts plus.

    The transistors and R3 may not be mounted, but if you need a bit more GND_Current,

    because the CMOS_OPAMP can not spend this, the two transistors with that Emitter_R can be used.

     

    image

     

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to geralds

    Thank you for the idea. I had a spare op amp, too!

     

    It wouldn't need the transistors, once the capacitor has charged the battery current is just under 2.5mA.

     

    An even simpler alternative would have been to use a second battery (I've got some 3V lithium coin cells that would have suited). I didn't think of that either.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to jc2048

    Jon,

     

    Another simple approach to a second supply is an isolated DC-to-DC supply to provide the opposite rail.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • geralds
    geralds over 7 years ago in reply to jc2048

    jc2048  wrote:

     

    Thank you for the idea. I had a spare op amp, too!

     

    It wouldn't need the transistors, once the capacitor has charged the battery current is just under 2.5mA.

    If you connect an empty capacitor ( eg. big electrolyte cap.), it will draw a bit more current then 2.5mA for few µs or up to ms.

    This can be more sink current than the OPAMP can drive.

    An even simpler alternative would have been to use a second battery (I've got some 3V lithium coin cells that would have suited).

    I didn't think of that either.

    The positive voltage can need other supply current than the negative supply current.

    So with two batteries it works well, but one of the both can be faster empty.

     

    As Gene mentioned:

    A DC-DC supply may be a fine solution. You would see the cost for your circuit as well.

    An 8 pin DC-DC converter mounted on a DIL or SIL socket is very cheap. It may cost about 3...5..6 EUR, or similar in USD.

    For example, you can generate from a 9V battery plus / minus 9V.

    The point of the other hand: the inrush current if you connect an empty capacitor on the test clips, hopefully that the DC-DC can supply this current.

    Also, if you toggle the capacitor on / off on the test clips, then a pump oscillation could occur, overloading the input of the instrumentation amplifier.

    Free wheel diodes may be needing on the + inputs of the amp.

    Similar to the charge-discharge curve of a capacitor, this can swing open looped. You can see that at the V-meter.

     

    Well fine project!

    Because busy my time, I didn't check the instrument amp. If I have time I will like to post a suggestion.

    I've bookmarked this web site, I'm looking forward very interested.

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to geralds

    The charging is through a resistor, and is never more than a milliamp, so I think the op amp would be fine.

     

    I might be concerned at the switching noise you'd get from a dc-dc converter. The whole thing was sensitive enough for me to put it in the tin can. On the bench it picks up a 51kHz triangular waveform from somewhere that I can't track down, though it seems to relate to the antistatic mat (which would just be coupling it - possibly from the mains earth).

     

    I'm not sure that shielding the board with a noise source inside the shield is the thing to do (as it stands, the battery is very quiet and there is no switching in the old op amp - it's not a no-drift chopper part).

     

    Thanks for the ideas. They may help anyone with a circuit to design that isn't quite so sensitive.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to genebren

    A good idea but...

     

    see my reply to Gerald below.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 7 years ago in reply to genebren

    A good idea but...

     

    see my reply to Gerald below.