Passive Components
  • Technologies
  • More
Passive Components
Forum Male/female pin converter?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 112 subscribers
  • Views 5367 views
  • Users 0 members are here
Related

Male/female pin converter?

madbilly
madbilly over 6 years ago

Hi everyone,

First, this is my first post in element14 so I don't know if there is a better subforum for my question - if there is, then mods please move it there.

 

I'm trying to find some pin converters, by which I mean something which will change a male pin into a female socket. This is primarily for stacking shield boards on top of a microcontroller board when I've got the wrong sense pins soldered in and don't want to change them. For example, I have two boards which I want to stack, both have male pins, so how do I connect them? I've looked around a lot of sites trying to find these but haven't succeeded yet and when I was thinking of where I could ask element14 seemed like the logical choice.

 

Helpful suggestions much appreciated.

Cheers image

  • Sign in to reply
  • Cancel

Top Replies

  • luislabmo
    luislabmo over 6 years ago +10
    Hello, I agree with others, maybe if you need an adapter for these kind of situations, pay good attention to the orientation, as usually parts that are stackable use stackable-female headers and most of…
  • shabaz
    shabaz over 6 years ago +6
    Hi, I don't think such a thing exists (maybe it does as some hobby item but I've not seen it), but there are a few other options if you don't wish to remove the pin header from one of the boards. The simplest…
  • beacon_dave
    beacon_dave over 6 years ago in reply to shabaz +5
    "Another option is to get hold of a couple of header sockets, and solder them back-to-back. It would be an ugly solution though." If you use separate header shells and female inserts, then you could crimp…
Parents
  • luislabmo
    luislabmo over 6 years ago

    Hello,

     

    I agree with others, maybe if you need an adapter for these kind of situations, pay good attention to the orientation, as usually parts that are stackable use stackable-female headers and most of the time are placed in the same orientation. Here are a few options to consider:

    • Change your shield boards to use stackable female headers, these are mainly used for your intended purpose, when used on a PCB they look like these
      image
    • For female-to-female connections use break-away headers
      image
    • For male-to-male connections SMD approach: I think you can make your own PCB and use SMD female headers on both sides connected with vias, like a type of sandwich, this way you can decide how many pins you need and by using SMD female headers, they can be perfectly aligned one on top of each other.
      image
    • For male-to-male connections, If you don't want to fiddle with SMD, well you can make your own PCB with two edges like in the picture below and solder two female headers on each side. The downside of this approach is that the spacing between the shields will be huge
      imageimage
    • Poor's man male-to-male connection, well the last resort is to use a piece of solderable PCB protoboard and offsett to female headers each on different side of the PCB. The downside of this one is that will offset your shields.

      OR
      use two right angle headers with the same PCB  (clip the terminals so don't interfere and solder only on one side), this approach will offset your shields but can greatly reduce the spacing between them
      imageimageimage

    Luis

    • Cancel
    • Vote Up +10 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • luislabmo
    luislabmo over 6 years ago

    Hello,

     

    I agree with others, maybe if you need an adapter for these kind of situations, pay good attention to the orientation, as usually parts that are stackable use stackable-female headers and most of the time are placed in the same orientation. Here are a few options to consider:

    • Change your shield boards to use stackable female headers, these are mainly used for your intended purpose, when used on a PCB they look like these
      image
    • For female-to-female connections use break-away headers
      image
    • For male-to-male connections SMD approach: I think you can make your own PCB and use SMD female headers on both sides connected with vias, like a type of sandwich, this way you can decide how many pins you need and by using SMD female headers, they can be perfectly aligned one on top of each other.
      image
    • For male-to-male connections, If you don't want to fiddle with SMD, well you can make your own PCB with two edges like in the picture below and solder two female headers on each side. The downside of this approach is that the spacing between the shields will be huge
      imageimage
    • Poor's man male-to-male connection, well the last resort is to use a piece of solderable PCB protoboard and offsett to female headers each on different side of the PCB. The downside of this one is that will offset your shields.

      OR
      use two right angle headers with the same PCB  (clip the terminals so don't interfere and solder only on one side), this approach will offset your shields but can greatly reduce the spacing between them
      imageimageimage

    Luis

    • Cancel
    • Vote Up +10 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 6 years ago in reply to luislabmo

    These are quite hard to find : ) I've wanted to get some for ages, but never found the magic search term! I thought they may be for wire-wrap, but not seen them on Farnell/Newark site. I had a couple of 40-way lengths of these but used it up over the past few years : (

    Sometimes I'll use the smaller ones and try to push the plastic portion into the center.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 6 years ago in reply to shabaz

    I tried few times and yes they are really hard to find with a good price (also the colored ones). I do get them from Pololu, Adafruit, Sparkfun, etc which usually get these kind specific parts from not so popular manufacturers but the thing with these providers is that they do their QC homework and do sell quality parts, so they have good coatings, LEDs will be all the same brightness, leads won't rust over time, etc.

    Try "double sided male headers", "equal length pin header" or "extra-long ping header" I found many results with these terms and maybe few of those will be based in the UK.


    Luis

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to luislabmo

    Thanks! I've just seen them:

    40 Pin Double sided Straight Header 0.1in | 1065 | Pololu

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 6 years ago in reply to luislabmo

    Thanks Luis,

     

    I too have been searching for the double male headers for a long time. I had actually given up but your post identifying the vendor Pololu allowed me to find some. I have placed my order and I am happy.

     

    John

    • Cancel
    • Vote Up +4 Vote Down