Passive Components
  • Technologies
  • More
Passive Components
Forum Male/female pin converter?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 112 subscribers
  • Views 5355 views
  • Users 0 members are here
Related

Male/female pin converter?

madbilly
madbilly over 6 years ago

Hi everyone,

First, this is my first post in element14 so I don't know if there is a better subforum for my question - if there is, then mods please move it there.

 

I'm trying to find some pin converters, by which I mean something which will change a male pin into a female socket. This is primarily for stacking shield boards on top of a microcontroller board when I've got the wrong sense pins soldered in and don't want to change them. For example, I have two boards which I want to stack, both have male pins, so how do I connect them? I've looked around a lot of sites trying to find these but haven't succeeded yet and when I was thinking of where I could ask element14 seemed like the logical choice.

 

Helpful suggestions much appreciated.

Cheers image

  • Sign in to reply
  • Cancel

Top Replies

  • luislabmo
    luislabmo over 6 years ago +10
    Hello, I agree with others, maybe if you need an adapter for these kind of situations, pay good attention to the orientation, as usually parts that are stackable use stackable-female headers and most of…
  • shabaz
    shabaz over 6 years ago +6
    Hi, I don't think such a thing exists (maybe it does as some hobby item but I've not seen it), but there are a few other options if you don't wish to remove the pin header from one of the boards. The simplest…
  • beacon_dave
    beacon_dave over 6 years ago in reply to shabaz +5
    "Another option is to get hold of a couple of header sockets, and solder them back-to-back. It would be an ugly solution though." If you use separate header shells and female inserts, then you could crimp…
Parents
  • madbilly
    madbilly over 6 years ago

    Hi all,

    Thanks for the great suggestions, I think that if I can't make one of these work then there's no helping me! image

     

    One remark on replacing male headers with female ones - I've previously tried this and found them very difficult to remove. Since the pins are connected to each other, one pin cannot be easily removed without the others, and removing all the solder to detach them all before removing the whole assembly is very difficult. I tried to just push the pins through when the solder was molten, but this resulted in damage to a board so I've not tried it again.

     

    I'm still very surprised that such a simple and convenient thing as a male to male connection adapter doesn't exist off the shelf, but since it doesn't I have to consider all other options.

     

    Cheers image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 6 years ago in reply to madbilly

    To desolder headers this is what I'd do: use a flush-cutter to clip the pins as much as you can from the soldered side, then remove the header plastic retainer -use the flush cutter as well for this, the pins now are individually held just by the solder. Then desolder them one by one (they are going to fall by themselves or use a tweezer to help removing them), use a solder pump in this step to desolder them and/or to clean the pads after. If you try to desolder the header without disassembling it, chances are you will end up burning the copper traces.

     

    Luis

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • madbilly
    madbilly over 6 years ago in reply to luislabmo

    That's exactly what happened - the traces got damaged image Thanks for the suggestions for doing it more efficiently image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to luislabmo

    Sounds like a voice of experience.

     

    My soldering career is long behind me. I assume the process of solder sucking  each pin individually with a good vacuum device doesn't work?

     

    I seem to recall this was the process for removing IC's. Now the pin on an IC moves slightly when pressure is applied. Maybe not so much with a connector leaving solder behind that binds.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 6 years ago in reply to colporteur

    In my experience, it requires a good soldering pump to do it without extra effort -like you said. The popular solder pumps (the ones with nylon tip that most people have) will probably give you extra work image

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • luislabmo
    luislabmo over 6 years ago in reply to colporteur

    In my experience, it requires a good soldering pump to do it without extra effort -like you said. The popular solder pumps (the ones with nylon tip that most people have) will probably give you extra work image

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 6 years ago in reply to luislabmo

    Those blue plastic single action pumps are fine for a small job but for professional solder removal a more robust device with a steady vacuum is required.

     

    I do like the idea of cropping the header before removal. Definitely make it easier removing a pin at a time.