Passive Components
  • Technologies
  • More
Passive Components
Forum Unusual Variable Inductor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 111 subscribers
  • Views 3982 views
  • Users 0 members are here
  • variable_inductor
Related

Unusual Variable Inductor

jw0752
jw0752 over 11 years ago

I was digging through my electronics graveyard and I found this interesting variable inductor. It has a ceramic drum wound with 14 gauge silver alloy wire. I measure a minimum to max range of 1uH to 12uH. As the drum is turned a small idler wheel rolls over the coil as a variable tap changing the amount of the coil that is included in the circuit. I was hoping that someone could tell me more about its original application. The square plates on the frame are 6.2 cm on a side and the length of the body is 9.5 cm. The front main shaft is coupled to the drum with an insulated universal joint. I see a shadow on the ceramic where there was likely a label at one time but it is gone now. If I can get a little more information about it I will put a tag on it so the next time someone runs across it there will not be a mystery.

 

image

 

image

 

image

 

image

 

Thanks John

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +2 verified
    To me, it looks like a medium-power 'roller inductor.' The gear makes me think it was intended to be operated by a motor. The most likely application was to tune an HF antenna. Yup, HF autotuner is my…
  • D_Hersey
    D_Hersey over 11 years ago +2
    I think due to its scale that this was used on the transmit side to normalize the load. The application circuit would have been along these lines: Pi-Match | Electronics and Electrical Engineering Tools…
  • jw0752
    jw0752 over 11 years ago in reply to shabaz +1
    Hi Shabaz, I was thinking that the operator had to watch a meter and power the motors manually but if I understand you correctly the motors would auto tune the antenna using an algorithm. this is pretty…
Parents
  • balearicdynamics
    0 balearicdynamics over 11 years ago

    Hi John,

     

    D_Hersey wrote


    The most likely application was to tune an HF antenna.  Yup, HF autotuner is my guess.  Probably tunes a resonant trap to keep the RF load around 50 ohms as the amp sees it.


    I agree with him, as I saw some of these in-action. About the gear - as far as what I saw - maybe a motor for big motorised antennas where the inductor rotates synched with the antenna too. Maybe considered the "ancient" motorised satellite dish image

    A simplified version it an air insulated inductor to tune frequencies on Germanium based radios. This is one of the first radios I have experimented with.


    Enrico



    imageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to balearicdynamics

    Hi Erico,

    Thanks for posting the interesting tuning box. I never thought about a tightening helical coil as a variable inductor before but  the physics says it will work.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to balearicdynamics

    Hi Erico,

    Thanks for posting the interesting tuning box. I never thought about a tightening helical coil as a variable inductor before but  the physics says it will work.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to jw0752

    Hi John,

    this strange "circuit" and the variable capacitor made me crazy too for a lot of time when I discovered this. And the strange is that it worked. I heard for hours incredible transmissions with this primitive radio image

     

    Enrico