Passive Components
  • Technologies
  • More
Passive Components
Forum LM 339 Comparator Question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 111 subscribers
  • Views 2955 views
  • Users 0 members are here
  • lm339
Related

LM 339 Comparator Question

jw0752
jw0752 over 11 years ago

Does anyone know if the unused inputs of an LM339 quad comparator need to be stabilized and if so what is the procedure? Since the outputs are open collector I suspect it is ok to leave them floating. I have checked my data sheets but I can't find anything about the unused inputs.

 

Thanks John

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 11 years ago +1 suggested
    It should be okay to leave them floating - there should be no excessive current conditions, but it looks like the internal circuit might use a bit more current when the output is low - it is hard to tell…
  • johnbeetem
    johnbeetem over 11 years ago +1 verified
    I would suggest pulling up the unused +in and pulling down the unused -in. That way your open-collector outputs are switched off and there's no internal switching generated by noise. JMO/YMMV
  • D_Hersey
    D_Hersey over 11 years ago +1
    Often, John, upon a little meditation, we can find a use for those unused comparators. They can be used to set up a warning light with an LED, for example.
Parents
  • dougw
    0 dougw over 11 years ago

    It should be okay to leave them floating - there should be no excessive current conditions, but it looks like the internal circuit might use a bit more current when the output is low - it is hard to tell because the internal schematic does not show all components in the chip. If there is noise getting to floating inputs, it could cause random switching internally, which could inject some small noise on the power supply.

    Doug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago

    It should be okay to leave them floating - there should be no excessive current conditions, but it looks like the internal circuit might use a bit more current when the output is low - it is hard to tell because the internal schematic does not show all components in the chip. If there is noise getting to floating inputs, it could cause random switching internally, which could inject some small noise on the power supply.

    Doug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 11 years ago in reply to dougw

    Hi Doug,

    Thank you for the prompt reply. I use these LM339s all the time but most of the time the application is just an experiment and I don't mind floating inputs. This time the application is a little more important to me so I wanted to make sure that I was following proper protocols.

    John