Passive Components
  • Technologies
  • More
Passive Components
Forum Overvoltage protection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 8 answers
  • Subscribers 111 subscribers
  • Views 2031 views
  • Users 0 members are here
Related

Overvoltage protection

e14 Contributor
e14 Contributor over 10 years ago

I have a problem with a variable ac wind generator

(15kW) which keeps blowing rectifiers. It normally generates at 300-350 v but can on a gust momentarily go over 400 which is the limit on the rectifiers which feed the inverters for onward network transmission.  I have rigged up, using a crouzet voltage control relay linked to a contactor, a bypass to protect inverters but it occurs to me that a capacitor bank or super cap would be able to 'absorb' the gust energy so;

am i correct in this assumption? if no, any suggestions for alternatives.  If yes, how do we size them and are we talking series or parallel? What would be the likely pitfalls/adverse consequences?!

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor +2
    current flow in windings is already near max on the gusts That does tend to limit your options a little. As I understand you can't reduce the load as that will tend to overspeed the blades, resulting…
  • jw0752
    jw0752 over 10 years ago +1 suggested
    Hi Ken, I know very little about wind mills but it seems to me that adding mass to the rotor would slow the reaction to wind gusts and even store some of the energy from the gust and spread it out over…
  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor +1 suggested
    Hi Ken, I do not see the capacitors as a solution to your problem. They would have to be on the rectified side of the diodes so they would actually be an increase in load at the time of stress. One solution…
Parents
  • mcb1
    0 mcb1 over 10 years ago

    It normally generates at 300-350 v but can on a gust momentarily go over 400

    AC or DC?

     

    The better method would be to detect the voltage and dump a large load onto it.

    I presume sustained winds cause the blades to feather or rotate to keep it within the design speed.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 10 years ago

    It normally generates at 300-350 v but can on a gust momentarily go over 400

    AC or DC?

     

    The better method would be to detect the voltage and dump a large load onto it.

    I presume sustained winds cause the blades to feather or rotate to keep it within the design speed.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer