Passive Components
  • Technologies
  • More
Passive Components
Forum use of capacitor to store sunlight energy
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 3 answers
  • Subscribers 109 subscribers
  • Views 2829 views
  • Users 0 members are here
  • capacitor
  • passives_featured
Related

use of capacitor to store sunlight energy

e14 Contributor
e14 Contributor over 10 years ago

Capacitor is used for storing the charge .

..cann't we use it for storing the energy which we are getting from sunlight \

...light which is coming from sun /..falling on silicon plate .

.electrons are emitting from the plate and this charge we want to store in  Capacitor ..

..Can we do that ? and for getting more electrons at a time can we also use a lens ..

..if si plate will be on the focus of the lens ..light which is coming through infinite .

.will be focused on focus center(plate)...so maximum electrons will be ejected can we do this ...if yes then reply pls and how ...i m making project on this ...thank u

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 7 years ago +4 suggested
    Hi Hari, Yes the photo voltaic energy produced by sunlight on a photo cell (solar cell) can be stored in a capacitor at least to the limit of the capacitor. The amount of energy that a capacitor can store…
  • DAB
    DAB over 7 years ago +2 suggested
    Hi Han, The problem with capacitors is charge storage capability. It takes a lot of capacitors to store the same amount of charge that a rechargeable battery contains. You just cannot beat batteries for…
  • Gough Lui
    Gough Lui over 7 years ago +1 suggested
    As others have mentioned, capacitors are not great for storing large amounts of charge (they're not energy dense), and they're not good for storing charge over long periods (they leak charge). More than…
Parents
  • jw0752
    0 jw0752 over 7 years ago

    Hi Hari,

     

    Yes the photo voltaic energy produced by sunlight on a photo cell (solar cell) can be stored in a capacitor at least to the limit of the capacitor. The amount of energy that a capacitor can store has been improving but it still is less than can be stored in the comparable cost of batteries. Batteries also provide an easier source for recovery of the energy for a practical use. When the energy is being recovered from a capacitor for use the voltage drops steadily. This means that special circuits must be used to maintain a steady voltage level. A battery on the other had has a tendency to maintain a much more level voltage output and thus requires less circuitry to make it useful. Sometimes Batteries and capacitors are used together in special cases as the capacitors can deliver a higher instantaneous power while the batteries a good for the long haul. In reference to concentrating sunlight with a lens this is practical in only a limited sense. As light intensity is increased on a Solar Cell the output does not track in a linear fashion. There will come a point where more sunlight will not produce more current. The cost of large lenses is also likely to be more expensive than just purchasing a greater surface area of solar cells. This is why we see roof tops covered with solar cells and not just one small solar cell and a big lens.

     

    It is important to the advancement of our knowledge that experimenters like yourself conduct experiments and make new innovations. Please continue to do this.

     

    One other consideration is efficiency. Efficiency is a measure of how well we have taken a particular quantity of energy and converted it to a different form. The only 100% conversion is to heat. A good example is your example of the solar cell. I will make up some numbers to illustrate this. Let's say that 100 joules of solar energy fall on your solar cells. Of this 100 Joules perhaps 20 Joules are converted to electricity and the other 80 joules is dissipated as heat into the environment. Now we have 20 joules of energy that we are going to store in a capacitor or a battery. In the case of the capacitor this energy is going to be stored as potential energy in an electric field. In the case of a battery the energy will be stored as potential energy in a chemical system. Both of these are not 100 % efficient so between the loss to heat or other parasitic going in and the loss to heat coming out we may eventually have 10 joules of energy to deliver to the final application where the available energy will be turned into light, sound, motion, an other form of energy, and ultimately to heat. The most efficient thing to do is always eliminate as many conversions as possible in the chain from our energy source to our application.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 7 years ago

    Hi Hari,

     

    Yes the photo voltaic energy produced by sunlight on a photo cell (solar cell) can be stored in a capacitor at least to the limit of the capacitor. The amount of energy that a capacitor can store has been improving but it still is less than can be stored in the comparable cost of batteries. Batteries also provide an easier source for recovery of the energy for a practical use. When the energy is being recovered from a capacitor for use the voltage drops steadily. This means that special circuits must be used to maintain a steady voltage level. A battery on the other had has a tendency to maintain a much more level voltage output and thus requires less circuitry to make it useful. Sometimes Batteries and capacitors are used together in special cases as the capacitors can deliver a higher instantaneous power while the batteries a good for the long haul. In reference to concentrating sunlight with a lens this is practical in only a limited sense. As light intensity is increased on a Solar Cell the output does not track in a linear fashion. There will come a point where more sunlight will not produce more current. The cost of large lenses is also likely to be more expensive than just purchasing a greater surface area of solar cells. This is why we see roof tops covered with solar cells and not just one small solar cell and a big lens.

     

    It is important to the advancement of our knowledge that experimenters like yourself conduct experiments and make new innovations. Please continue to do this.

     

    One other consideration is efficiency. Efficiency is a measure of how well we have taken a particular quantity of energy and converted it to a different form. The only 100% conversion is to heat. A good example is your example of the solar cell. I will make up some numbers to illustrate this. Let's say that 100 joules of solar energy fall on your solar cells. Of this 100 Joules perhaps 20 Joules are converted to electricity and the other 80 joules is dissipated as heat into the environment. Now we have 20 joules of energy that we are going to store in a capacitor or a battery. In the case of the capacitor this energy is going to be stored as potential energy in an electric field. In the case of a battery the energy will be stored as potential energy in a chemical system. Both of these are not 100 % efficient so between the loss to heat or other parasitic going in and the loss to heat coming out we may eventually have 10 joules of energy to deliver to the final application where the available energy will be turned into light, sound, motion, an other form of energy, and ultimately to heat. The most efficient thing to do is always eliminate as many conversions as possible in the chain from our energy source to our application.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer