Passive Components
  • Technologies
  • More
Passive Components
Forum What is the Purpose of Resistor R1 in this Circuit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 6 answers
  • Subscribers 109 subscribers
  • Views 5345 views
  • Users 0 members are here
  • power_supply
Related

What is the Purpose of Resistor R1 in this Circuit

jw0752
jw0752 over 7 years ago

This last weekend I had to repair a simple circuit that was designed to turn a vacuum system on and off with the alternate push of a SPST momentary switch. Here is the circuit that I worked on.

 

image

The problem turned out to be that the manufacturer had the C1 capacitor installed reversed polarity. Removal of the capacitor and replacement with  a new one in the proper polarity solved the problem.

 

My question concerns the 150 Ohm R! resistor as I have never seen a power supply with the negative lead of the filter capacitor held above ground. Can someone give me some information on what the designer's reason for the inclusion of R1 in this circuit might have been?

 

Thanks John

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +6 suggested
    Perhaps it is to limit inrush current and avoid stressing the diode or upstream fuses? It could also be to limit discharge current when power is removed (to avoid stressing the module's protection diodes…
  • jw0752
    jw0752 over 7 years ago +5
    Here is perhaps a better image of the schematic: John
  • shabaz
    shabaz over 7 years ago in reply to jw0752 +5 suggested
    Hi John! I'm not sure, but maybe the transformer is very small and as Doug says, it could be to reduce high current draw briefly. Those types of relays are very cool.. I think they maybe referred as step…
Parents
  • gecoz
    0 gecoz over 7 years ago

    Hi John,

     

    I think the meaning of R1 is to reduce the power consumption of the relay once the contacts are triggered closed. The relay coil will have a defined operating current, needed to switch it to close, but once the contacts are closed, the current required by the coil to keep the relay contacts closed is normally sensibly lower than the operating current. Adding R1 will reduce the current flowing into the coil, thus reducing power consumption.

     

    There is a drawback though, but in your case I think can be ignored: adding R1 in series to C1 will make the capacitor time constant longer, hence limiting the switching speed of the relay.

     

    Fabio

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gecoz
    0 gecoz over 7 years ago

    Hi John,

     

    I think the meaning of R1 is to reduce the power consumption of the relay once the contacts are triggered closed. The relay coil will have a defined operating current, needed to switch it to close, but once the contacts are closed, the current required by the coil to keep the relay contacts closed is normally sensibly lower than the operating current. Adding R1 will reduce the current flowing into the coil, thus reducing power consumption.

     

    There is a drawback though, but in your case I think can be ignored: adding R1 in series to C1 will make the capacitor time constant longer, hence limiting the switching speed of the relay.

     

    Fabio

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer