Passive Components
  • Technologies
  • More
Passive Components
Forum Relay Delay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 111 subscribers
  • Views 1651 views
  • Users 0 members are here
  • relay
Related

Relay Delay

nick123
nick123 over 11 years ago

I want to make a delay, so that when the circuit turns on, it takes a while for it to come on.

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +2
    There are a lot of topological possibilities for a circuit that creates a delay. Let me abstract this discussion a little bit from your application. You can extend the delay period for just about any setup…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Nick, there are commercial products available that do this. they are called Delay on Make Relays. I have worked with them in the past. Some come with DIP switches that can be set to program the number of seconds of delay between the powering of the circuit and when the relay closes and actually turns it on. There is a small preliminary current that has to pass through the module to power its internal electronics while it times out and closes the main sircuit allowing the circuit to come up to load amperage.

     

    http://www.newark.com/artisan-controls/438usas/solid-state-timer-1024sec-288vac/dp/86K9984

     

    This unit will work on 19V all the way to 288V AC or DC.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago

    Hi Nick, there are commercial products available that do this. they are called Delay on Make Relays. I have worked with them in the past. Some come with DIP switches that can be set to program the number of seconds of delay between the powering of the circuit and when the relay closes and actually turns it on. There is a small preliminary current that has to pass through the module to power its internal electronics while it times out and closes the main sircuit allowing the circuit to come up to load amperage.

     

    http://www.newark.com/artisan-controls/438usas/solid-state-timer-1024sec-288vac/dp/86K9984

     

    This unit will work on 19V all the way to 288V AC or DC.

     

    John