Passive Components
  • Technologies
  • More
Passive Components
Forum How can I deal with resistors when I'm colorblind?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 47 replies
  • Answers 4 answers
  • Subscribers 120 subscribers
  • Views 15714 views
  • Users 0 members are here
  • green
  • identification
  • color
  • colorblind
  • component
  • red
Related

How can I deal with resistors when I'm colorblind?

4ringfan
4ringfan over 11 years ago

Hey guys, Mike Wiltrout here.  I believe many of you may know my father, John Wiltrout.

 

This really is not much of an introduction post, but it is my first on E-14.  It is picture laden so I apologize for that ahead of time.  I did, however, feel like it would be an interesting topic that some of you might be able to help me with, so here goes!

 

In my early childhood, I recall wanting to be a fireman.  One day, my mother took me in to the clinic for a school physical.  It was then that the doctor showed me a series of images with different color dots on them to determine if I was colorblind.  Supposedly somewhere in the mix of dots on each image was supposed to be a number that I was to recite when I could make it out.  Unfortunately for me I could make very few of them out.  Below is an example of just such a chart and on that chart below I can really only make out the '12' in the upper right corner.  It was then that the doctor began telling me about all of the careers that I would never be able to pursue.  Included in that list was fireman.  When I asked the doctor why I would not be able to be a fireman, he told me that firemen need to be able to see colors to be able to tell how hot a flame was.  So I left the doctor's office that day a little bit sad and discouraged.

image

My father, being the troubleshooter that he is, set out to try and help me with my colorblind condition.  He picked up color swatches in hopes that I might be able to "re-learn" the colors or at least be able to use the color swatches to compare against colors I wanted to know.  Turns out it just doesn't work that way.  The problem comes with being unable to differentiate.  Red can look like orange, orange can look like yellow, yellow can look like green, green can look like blue, and so on.  ORANGE means STOP and WHITE means GO!  As a teen, I was interested in flying and wanted to get into the Air Force Academy, but pilots need to be able to see colors so they can tell if a plane is coming at them or flying away from them using colors on the wing and tail.  I then considered the National Guard, where I was told that I could not be an engineer and that the ONLY military career paths that were open to me were about few different ones: a chaplain, a draftsman, or an infantryman.  They wouldn't even let me be a cook because I cannot tell if meat is raw or cooked.  Anyhow, you get the idea, being color blind can be a challenge.  My wife finally made me get rid of my favorite blue office chair, because she could no longer stand the "hideous purple thing."

 

So, here is and has been my dilemma.  How do I differentiate and identify the various color coded resistors?



image


My solutions so far consist of the following:

 

  • GET A BUDDY TO HELP ME - Preferably a buddy who is also not colorblind, but while a buddy might be able to help me sort a new collection of resistors into bins, he isn't going to be attached to my hip when I need a resistor identified on a project that I'm working on at 3AM.image
  • MEASURE THE RESISTOR USING A MULTIMETER - This may work to identify a resistor outside of a circuit, but it also does not take into account any tolerances of the resistor, which I also cannot discern.  I do not want to de-solder a leg on each resistor I need to measure on a PCB, either.
    image
  • LABEL THE RESISTORS - This will work if I buy resistors that are in label pre-packaged bags and I am able to label them right away.  I probably would look to label them according to either European or SMT standards in order to keep the labels as small as possible.  This method takes a considerable amount if time, and I will probably only use it for prototyping.
    image
  • PREMARKED RESISTORS - Some resistors like SMT resistors have their values printed on them.  These I can figure out.
  • VISUAL COMPUTER AIDED ANALYSIS - Another idea that I had was to use either a camera, or a USB microscope to "scan" the resistor.  The image could then be dropped into a computer program that would orient the resistor and scan the color bands displaying a value in Ohms and providing me the tolerance.  I have no experience with any program that can automatic manipulation and color matching, so I'm stuck there.
  • FIX MYSELF? - The last idea would be to somehow fix myself with some type of contacts, glasses, or other medical method.  (Again, not my field of expertise.)

 

The problem is not limited to resistors, either.  I'm thinking a career in bomb disposal sounds pretty interesting, "Should I cut the RED wire or the BLUE wire?"

 

So lets hear some suggestions!  GO!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 11 years ago in reply to 4ringfan +4
    Hi Mike, I'm currently immersed in some pretty heavy projects, so I don't have much time to devote to this, but I just wrote a quick program in VB6 that will show the color of any pixel on the screen …
  • valdaquendë
    valdaquendë over 9 years ago +4 suggested
    As a color-blind individual myself, I've had to struggle with this for quite a while. I read about ReScan, on this site and others but it is PC/Android only and requires a bit of putzing to install and…
  • dougw
    dougw over 11 years ago +3 suggested
    Maybe this app would help... Optical recognition of resistor codes | Labrigger from Nothing Labs (Rich Olson) Resistor Photo ID
Parents
  • mcb1
    0 mcb1 over 11 years ago

    Mike

    You don't need to be colour blind to have trouble.

    Us older ones can tell you that the smaller they are, the worse it is.

     

    However having said that some of the cheap resistors from Asian sources have colours that are 'close' to the proper, but sometimes not.

    We have a Xmas Tree project for pupils and appart from a process of elimination, the meter often comes out.

     

    I'm wondering if filters in front of the resistor and the use of UV/IR light might make some colours there and others not.

    As for stocks, I can only suggest stick to the e27?? range and use the plastic bags the banks give out for change.

     

    SMT

    You're right they label them, but only the larger size ... I have some grains of sand that are apparently reistors. image

     

    Nice topic, welcome to the forum.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 4ringfan
    0 4ringfan over 11 years ago in reply to mcb1

    mcb,

     

    You aren't kidding!  I used to think it was funny when my old man would prefer parts catalogs with LARGE print in them.  Now I find myself having to look over the top of my glasses when I work on something close and it isn't so funny any more.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 4ringfan
    0 4ringfan over 11 years ago in reply to mcb1

    mcb,

     

    You aren't kidding!  I used to think it was funny when my old man would prefer parts catalogs with LARGE print in them.  Now I find myself having to look over the top of my glasses when I work on something close and it isn't so funny any more.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 11 years ago in reply to 4ringfan

    I'm the opposite.

    The arms are only so long, but when it's finally in focus it's too small to read ...image

     

    Mark