Passive Components
  • Technologies
  • More
Passive Components
Forum Need to replace resistor 900 ohms / % Tolerance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 41 replies
  • Subscribers 108 subscribers
  • Views 11557 views
  • Users 0 members are here
Related

Need to replace resistor 900 ohms / % Tolerance

Alex-andre
Alex-andre over 3 years ago
Hello there,

I need to replace this resistor which appears to be a 900 ohm with a % tolerance. (4 rings = Black / White / Red / Silver or Grey and around 25mm long)

I bought one with almost same features (OHMITE OX102KE Through Hole Resistor, 1K ohm, OX, 1W, ±10%, Axial, 300V) but it doesn't fit, it's far too small compare to the one I need to replace. Do you have any suggestion where to buy or how to replace it ?

I attached a picture below.

Thanks a lot

Aleximage
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 3 years ago in reply to dougw +5
    Hi Doug, I'm doing good. Glad to see so many old friends still around.
  • jw0752
    jw0752 over 3 years ago +3
    Based on my experience with this style relay it is highly probable that the resistor is across the Normally Open relay contacts and serves as a soft start to the load. As configured it would current limit…
  • Gough Lui
    Gough Lui over 3 years ago +1
    Do you have any information about the power rating? As long as the power rating of the replacement is the same or greater than the original, it doesn't really matter that it is physically smaller. You…
Parents
  • Gough Lui
    0 Gough Lui over 3 years ago

    Do you have any information about the power rating? As long as the power rating of the replacement is the same or greater than the original, it doesn't really matter that it is physically smaller. You can just bend the leads as appropriate to fit.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Alex-andre
    0 Alex-andre over 3 years ago in reply to Gough Lui

    thx for the quick reply, I'm not an expert so apologize if I misunderstand. :-)
    The mother board indicate 1V and booth resistors are made for 1V.
    Should I measure something else? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 3 years ago in reply to Alex-andre

    That response doesn't make sense - if you're referring to the writing - V1.0 means version 1.0. Or do you mean you measured 1V over the resistor (which seems to be rated 1kOhm, 10% tolerance)?

    Do you have the bill of materials for the board? Or a list of parts that indicates the power rating of the original resistor? This is in watts. Common resistor sizes are 1/4W, 1/2W, 1W, 2W, 5W, 10W, 25W etc. You might be able to guess by physical size, but that is not always reliable. If the existing one you have is too physically small and you are concerned it doesn't have enough power rating, you might just opt to order one with a larger power rating as it will be physically larger.

    When replacing resistors, you don't only need to match the ohms rating and have equal or better tolerance. You also need to have equal or greater power rating and equal or better voltage rating as well. Some resistors also serve special functions (e.g. fusible resistors) which must be replaced with the same type to maintain safety.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 3 years ago in reply to Alex-andre

    That response doesn't make sense - if you're referring to the writing - V1.0 means version 1.0. Or do you mean you measured 1V over the resistor (which seems to be rated 1kOhm, 10% tolerance)?

    Do you have the bill of materials for the board? Or a list of parts that indicates the power rating of the original resistor? This is in watts. Common resistor sizes are 1/4W, 1/2W, 1W, 2W, 5W, 10W, 25W etc. You might be able to guess by physical size, but that is not always reliable. If the existing one you have is too physically small and you are concerned it doesn't have enough power rating, you might just opt to order one with a larger power rating as it will be physically larger.

    When replacing resistors, you don't only need to match the ohms rating and have equal or better tolerance. You also need to have equal or greater power rating and equal or better voltage rating as well. Some resistors also serve special functions (e.g. fusible resistors) which must be replaced with the same type to maintain safety.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Alex-andre
    0 Alex-andre over 3 years ago in reply to Gough Lui

    Thanks for your reply. 
    I do not have the bill of materials for the board, could I measure the power rating from the board directly ? 

    ffyi the resistor come from the cardboard of this product --> https://www.heatpumps4pools.com/myfiles/file/Clever-Pool-Pump-Inverter-Installation-manual.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 3 years ago in reply to Alex-andre

    No. Power ratings cannot be measured from the board. You need to understand what the resistor is doing and the circuitry to be able to reverse engineer the power rating requirement if you don't know the exact part that is needed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Alex-andre
    0 Alex-andre over 3 years ago in reply to Gough Lui

    Ok, thx I need to investigate further then.