Passive Components
  • Technologies
  • More
Passive Components
Forum Need to replace resistor 900 ohms / % Tolerance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 41 replies
  • Subscribers 108 subscribers
  • Views 11292 views
  • Users 0 members are here
Related

Need to replace resistor 900 ohms / % Tolerance

Alex-andre
Alex-andre over 3 years ago
Hello there,

I need to replace this resistor which appears to be a 900 ohm with a % tolerance. (4 rings = Black / White / Red / Silver or Grey and around 25mm long)

I bought one with almost same features (OHMITE OX102KE Through Hole Resistor, 1K ohm, OX, 1W, ±10%, Axial, 300V) but it doesn't fit, it's far too small compare to the one I need to replace. Do you have any suggestion where to buy or how to replace it ?

I attached a picture below.

Thanks a lot

Aleximage
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 3 years ago in reply to dougw +5
    Hi Doug, I'm doing good. Glad to see so many old friends still around.
  • jw0752
    jw0752 over 3 years ago +3
    Based on my experience with this style relay it is highly probable that the resistor is across the Normally Open relay contacts and serves as a soft start to the load. As configured it would current limit…
  • Gough Lui
    Gough Lui over 3 years ago +1
    Do you have any information about the power rating? As long as the power rating of the replacement is the same or greater than the original, it doesn't really matter that it is physically smaller. You…
Parents
  • robogary
    0 robogary over 3 years ago

    Another easy thing to try is to remove the 3 output wires to the motor , see if the problem goes away. Perhaps the output is grounded. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • robogary
    0 robogary over 3 years ago

    Another easy thing to try is to remove the 3 output wires to the motor , see if the problem goes away. Perhaps the output is grounded. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Alex-andre
    0 Alex-andre over 3 years ago in reply to robogary

    ok

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robogary
    0 robogary over 3 years ago in reply to Alex-andre

    if the problem goes away after removing the motor leads, use an ohmmeter to check each motor lead to ground. the readings should be well above 10 kohm. Measure ohms between the 3 motor leads, 1-2, 2-3, 1-3 they should be approximately the same. You could also check to see the pump motor shaft is not stuck or frozen.     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Alex-andre
    0 Alex-andre over 3 years ago in reply to robogary

    ok