Passive Components
  • Technologies
  • More
Passive Components
Forum Need to replace resistor 900 ohms / % Tolerance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 41 replies
  • Subscribers 108 subscribers
  • Views 11305 views
  • Users 0 members are here
Related

Need to replace resistor 900 ohms / % Tolerance

Alex-andre
Alex-andre over 3 years ago
Hello there,

I need to replace this resistor which appears to be a 900 ohm with a % tolerance. (4 rings = Black / White / Red / Silver or Grey and around 25mm long)

I bought one with almost same features (OHMITE OX102KE Through Hole Resistor, 1K ohm, OX, 1W, ±10%, Axial, 300V) but it doesn't fit, it's far too small compare to the one I need to replace. Do you have any suggestion where to buy or how to replace it ?

I attached a picture below.

Thanks a lot

Aleximage
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 3 years ago in reply to dougw +5
    Hi Doug, I'm doing good. Glad to see so many old friends still around.
  • jw0752
    jw0752 over 3 years ago +3
    Based on my experience with this style relay it is highly probable that the resistor is across the Normally Open relay contacts and serves as a soft start to the load. As configured it would current limit…
  • Gough Lui
    Gough Lui over 3 years ago +1
    Do you have any information about the power rating? As long as the power rating of the replacement is the same or greater than the original, it doesn't really matter that it is physically smaller. You…
Parents
  • dougw
    0 dougw over 3 years ago

    black-white-red-silver should be 92 ohms 10% tolerance (which is a bit strange, so it should be measured)
    It looks like a 2W, 3W or 5W resistor (I've seen all 3 ratings in this size)
    If it is a 24 V circuit, I would go with 5 W, If it is a 12 V circuit maybe 2 W is enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 3 years ago

    black-white-red-silver should be 92 ohms 10% tolerance (which is a bit strange, so it should be measured)
    It looks like a 2W, 3W or 5W resistor (I've seen all 3 ratings in this size)
    If it is a 24 V circuit, I would go with 5 W, If it is a 12 V circuit maybe 2 W is enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Alex-andre
    0 Alex-andre over 3 years ago in reply to dougw

    thx