Passive Components
  • Technologies
  • More
Passive Components
Forum Any help on the following low pass filter scenario would be very much appreciated.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 109 subscribers
  • Views 2555 views
  • Users 0 members are here
Related

Any help on the following low pass filter scenario would be very much appreciated.

k.morrow
k.morrow over 2 years ago

Objective: To build a shielded cable with a passive low pass filter to be used for connecting the ground connection of a typical US 120V socket or from an earth  ground rod to a bed sheet with silver threads in it for grounding or earthing purposes. The purpose is for the filter to eliminate any/all AC noise from going up the shielded cable and getting to the bed sheet.
For testing possible filter configurations I have a Fluke 179 True RMS multimeter and an old Hitachi V-152F-15MHz Oscope and a BK 3011B - 2 MHz Function generator.

My thoughts are to use a single resistor with an electrolytic capacitor so when measured with the multimeter in one direction I would measure the resistor value and in the other direction I would measure an infinite impedance.

I have explored several online low pass filter calculators:
www.redcrab-software.com/.../RC-Low-Pass-Filter
sim.okawa-denshi.jp/.../CRlowkeisan.htm
learningaboutelectronics.com/.../Low-pass-filter-calculator.php
markimicrowave.com/.../

I have a few questions:
1. Do I make the filter with a cutoff frequency of 60Hz or something very low like 1Hz or less?
2. Is an RC filter best or use an RLC or some other config?
3. Could the filter be better with a 2nd order (or 3rd, or 4th ...?).
4. For the filter connected to a shielded cable, are surface mount components better to use than leaded components?

Thank You!!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago +1
    If the only connection is ground, what are you filtering with respect to? I'm not sure you can do better than a direct connection to ground to minimize capacitive, inductive or RF coupling to the sheet…
  • anniel747
    anniel747 over 2 years ago

    A schematic of your intended connections please.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 2 years ago

    Please also explain "bed sheet" is this a sheet on a bed for sleeping  - if so there could be problems with safety.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago

    If the only connection is ground, what are you filtering with respect to? I'm not sure you can do better than a direct connection to ground to minimize capacitive, inductive or RF coupling to the sheet..

    Is ESD of concern? (because that would have a different solution)

    If there is no other specific ground reference, an in-line inductor might do something to minimize AC with respect to the natural ambient ground.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to michaelkellett

    michaelkellett This is actually a thing.  https://www.amazon.com/Grounding-Silver-Conductive-Earthing-Better/dp/B0CJJ8G1M1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 2 years ago in reply to dougw

    +1 to this. I'm absolutely not an expert, but if the cable is connected to ground, all "radiation" it might be subjected to, will be grounded just like any RF emissions picked up by the sheet itself. The cable won't be any different from the sheet, in a way, so I'm not sure any "shielding" or filtering is required at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • k.morrow
    k.morrow over 2 years ago

    I am trying to eliminate any AC noise that is on the house ground from going up the shielded cable to the conductive bed sheet.

    I have attached a picture of what I want to do.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • k.morrow
    k.morrow over 2 years ago in reply to k.morrow

    It is the same concept as hooking up an ESD mat except I'm trying to filter any and all noise on the cable from the wall outlet ground to the ESD mat.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 2 years ago in reply to k.morrow

    How did you measure that noise?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 2 years ago in reply to k.morrow

    Why the polarised capacitor?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to k.morrow

    The resistor is all you need for ESD. That capacitor is big enough to give you a jolt if you have built up static electricity. The cap may have bled off to ground but if you are charged up it will allow rapid current inrush as you touch the sheet and the cap charges up to your potential (possibly causing a spark)

    Other notes:

    Ground by definition has no AC on it, but of course it depends on where you measure from and if there is current flowing in the ground causing IR voltages.

    As mentioned a polarized cap isn't ideal for a situation where it is not clear what voltage polarity will be applied.

    The shield in the diagram is just ground - no part of it is floating. I'm not clear what the "floating" lead is connected to off in the direction of the sheet, but if it is the conductive sheet, then the rest of the circuit is shorted out and not doing anything. 

    If you are worried about ground faults causing a shock, maybe consider a ground fault interrupter (GFI).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>