Passive Components
  • Technologies
  • More
Passive Components
Forum Any help on the following low pass filter scenario would be very much appreciated.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 109 subscribers
  • Views 2557 views
  • Users 0 members are here
Related

Any help on the following low pass filter scenario would be very much appreciated.

k.morrow
k.morrow over 2 years ago

Objective: To build a shielded cable with a passive low pass filter to be used for connecting the ground connection of a typical US 120V socket or from an earth  ground rod to a bed sheet with silver threads in it for grounding or earthing purposes. The purpose is for the filter to eliminate any/all AC noise from going up the shielded cable and getting to the bed sheet.
For testing possible filter configurations I have a Fluke 179 True RMS multimeter and an old Hitachi V-152F-15MHz Oscope and a BK 3011B - 2 MHz Function generator.

My thoughts are to use a single resistor with an electrolytic capacitor so when measured with the multimeter in one direction I would measure the resistor value and in the other direction I would measure an infinite impedance.

I have explored several online low pass filter calculators:
www.redcrab-software.com/.../RC-Low-Pass-Filter
sim.okawa-denshi.jp/.../CRlowkeisan.htm
learningaboutelectronics.com/.../Low-pass-filter-calculator.php
markimicrowave.com/.../

I have a few questions:
1. Do I make the filter with a cutoff frequency of 60Hz or something very low like 1Hz or less?
2. Is an RC filter best or use an RLC or some other config?
3. Could the filter be better with a 2nd order (or 3rd, or 4th ...?).
4. For the filter connected to a shielded cable, are surface mount components better to use than leaded components?

Thank You!!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago +1
    If the only connection is ground, what are you filtering with respect to? I'm not sure you can do better than a direct connection to ground to minimize capacitive, inductive or RF coupling to the sheet…
Parents
  • dougw
    dougw over 2 years ago

    If the only connection is ground, what are you filtering with respect to? I'm not sure you can do better than a direct connection to ground to minimize capacitive, inductive or RF coupling to the sheet..

    Is ESD of concern? (because that would have a different solution)

    If there is no other specific ground reference, an in-line inductor might do something to minimize AC with respect to the natural ambient ground.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 2 years ago in reply to dougw

    +1 to this. I'm absolutely not an expert, but if the cable is connected to ground, all "radiation" it might be subjected to, will be grounded just like any RF emissions picked up by the sheet itself. The cable won't be any different from the sheet, in a way, so I'm not sure any "shielding" or filtering is required at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • battlecoder
    battlecoder over 2 years ago in reply to dougw

    +1 to this. I'm absolutely not an expert, but if the cable is connected to ground, all "radiation" it might be subjected to, will be grounded just like any RF emissions picked up by the sheet itself. The cable won't be any different from the sheet, in a way, so I'm not sure any "shielding" or filtering is required at all.