Passive Components
  • Technologies
  • More
Passive Components
Forum Any help on the following low pass filter scenario would be very much appreciated.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 109 subscribers
  • Views 2566 views
  • Users 0 members are here
Related

Any help on the following low pass filter scenario would be very much appreciated.

k.morrow
k.morrow over 2 years ago

Objective: To build a shielded cable with a passive low pass filter to be used for connecting the ground connection of a typical US 120V socket or from an earth  ground rod to a bed sheet with silver threads in it for grounding or earthing purposes. The purpose is for the filter to eliminate any/all AC noise from going up the shielded cable and getting to the bed sheet.
For testing possible filter configurations I have a Fluke 179 True RMS multimeter and an old Hitachi V-152F-15MHz Oscope and a BK 3011B - 2 MHz Function generator.

My thoughts are to use a single resistor with an electrolytic capacitor so when measured with the multimeter in one direction I would measure the resistor value and in the other direction I would measure an infinite impedance.

I have explored several online low pass filter calculators:
www.redcrab-software.com/.../RC-Low-Pass-Filter
sim.okawa-denshi.jp/.../CRlowkeisan.htm
learningaboutelectronics.com/.../Low-pass-filter-calculator.php
markimicrowave.com/.../

I have a few questions:
1. Do I make the filter with a cutoff frequency of 60Hz or something very low like 1Hz or less?
2. Is an RC filter best or use an RLC or some other config?
3. Could the filter be better with a 2nd order (or 3rd, or 4th ...?).
4. For the filter connected to a shielded cable, are surface mount components better to use than leaded components?

Thank You!!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago +1
    If the only connection is ground, what are you filtering with respect to? I'm not sure you can do better than a direct connection to ground to minimize capacitive, inductive or RF coupling to the sheet…
Parents
  • michaelkellett
    michaelkellett over 2 years ago

    Please also explain "bed sheet" is this a sheet on a bed for sleeping  - if so there could be problems with safety.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to michaelkellett

    michaelkellett This is actually a thing.  https://www.amazon.com/Grounding-Silver-Conductive-Earthing-Better/dp/B0CJJ8G1M1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 2 years ago in reply to kmikemoo

    Strewth !

    Thanks  kmikemoo

    Science:

    As far as RF is concerned it will make little difference to the electric field just above the "silver" sheet if you connect the ground wire or not.

    Why - because the inductance of the wire and the mains wiring in the house will have a high impedance to ground at RF.

    The usual analogy in EMC testing is that grounding a large conducting structure with a wire longer than couple of inches is like trying to push an elephant with a piece of wet string.

    Nonsense: (you were warned !!!)

    https://www.youtube.com/@groundedwellness4359

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 2 years ago in reply to kmikemoo

    Strewth !

    Thanks  kmikemoo

    Science:

    As far as RF is concerned it will make little difference to the electric field just above the "silver" sheet if you connect the ground wire or not.

    Why - because the inductance of the wire and the mains wiring in the house will have a high impedance to ground at RF.

    The usual analogy in EMC testing is that grounding a large conducting structure with a wire longer than couple of inches is like trying to push an elephant with a piece of wet string.

    Nonsense: (you were warned !!!)

    https://www.youtube.com/@groundedwellness4359

    MK