Passive Components
  • Technologies
  • More
Passive Components
Forum Please Help with the Identification of this Part
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 113 subscribers
  • Views 2511 views
  • Users 0 members are here
Related

Please Help with the Identification of this Part

jw0752
jw0752 over 8 years ago

While cleaning out the backroom of an Electronics Store we came across about 100 of these chips. I took them to the shop but I have not been able to determine what they are. Resistance readings are very high and capacitance readings are negligible. Hamlin is now owned by Littlefuse. The 8235 on each appears to be a date code which makes sense as all the other chips that were with this lot all came from the 1970s. Anyone have any ideas. I have tried to Google the image also with no results.

 

image

 

Thanks John

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 8 years ago in reply to jw0752 +8
    Perhaps the links were opened with series of high-current pulses.
  • jw0752
    jw0752 over 8 years ago in reply to jc2048 +8
    Hi Jon, I tested your hypothesis by charging a large capacitor to 50 volts and discharging it into three of the 130 ohm links to pins 10 and 12. The resistive links were opened in all cases with almost…
  • jw0752
    jw0752 over 8 years ago +6
    Thank You, Fred27 balearicdynamics mcb1 DaveMcLaughlin , I have taken your advice and I have sacrificed a couple of the components to discover their mystery ID. Once the veneer was removed I could see…
Parents
  • jw0752
    jw0752 over 8 years ago

    Thank You,  Fred27 balearicdynamics  mcb1  DaveMcLaughlin ,

     

    I have taken your advice and I have sacrificed a couple of the components to discover their mystery ID. Once the veneer was removed I could see that it was laid out as a resistor array.

     

    image

    Pin 16 comes in as a metal trace that runs down the center of the chips. Laid over the top are black resistive material to each of the remaining 15 pins. Except for the resistive material to pins 10 and 12 the material has been cut with a ? laser on all the other pins. The apparent intent here was not to produce good quality resistors or good quality cuts.. Here is a close up of the chip at the right.

     

    image

    If you look closely you will see that only Pins 10 and 12 do not show the cut extending across the material. Further the cuts that are across the material of the other pins are poorly done. Actual resistance can range from 200K all the way to OL and none of the readings are stable except the reading on Pins 10 and 12. When I tried to read these unstable resistances with the megger they all showed low resistance at 100 V. None of the resistances, even those on Pins 10 and 12 are consistent from chip to chip. Here is a chart that I made of 3 random chips to show the resistances between the common pin 16 and each of the other pins. The ohm readings are in black.

     

    image

     

    Sorry it isn't a little clearer but you can click on it to enlarge it. Note that the common to pin resistance in black is not consistent between chips including the pin 10 and 12 readings. My conclusion at this point was that the actual resistances do not matter as long as there is a large difference between the cut traces and the not cut traces. These chips are a form of cheap factory programmable DIP Shunt. I set up a test circuit where I tied the common of the three chips to ground and then I put a 10K pullup resistor between a 5 volt power supply and my meter DC voltage probe. I then probed each pin on each chip and took the readings and wrote them in red on the chart. All Pins read High (close to 5 volts) except the Pins 10 and 12 on each chip which read 0.06 Volts.

     

    Perhaps a manufacturer determined that it would be cheaper to order programming shunts in this manner as opposed to using more expensive switches or more labor intensive punch out shunts. The answer is probably lost in the past.

     

    Thank you to those who responded and gave me the help to pursue this to a more understandable conclusion.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 8 years ago in reply to jw0752

    I was wondering if these resistors were to form a part of a DAC/ADC chain. Also resistors of this size are like 50v breakdown in SMD parts (all a bit approximate!!) so you may of damaged them at 100v or at least have to allow for an amount of breakdown in your values!

     

    John A

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to Problemchild
    Also resistors of this size are like 50v breakdown in SMD parts

    I was thinking that many of the circuits these would have been used in would be 5v or at worst 12v.

    Personally I would have used 15-20v to prove the function.

     

    They are an interesting device.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 8 years ago in reply to Problemchild

    Hi John,

    Anything is possible. The reason my analysis went the way it did was that the resistors all have a common lead and each of the several chips that I tested had the same branches damaged so that their resistances were anywhere from 300K to OL. The 2 resistors on each chip that are still intact have poor consistency from chip to chip with resistances of 130 to 150 ohms typical. It seemed to me that the only think important to the application must have been either a very high resistance or a relatively low one and this sound a lot like digital. I didn't try the 100 volt megger until I had taken lots of measurements with the fluke meter. The instability of the high readings I was getting made me want to verify and so I tried the megger. I would get resistance readings on the Fluke that would wander 1 meg in either direction on some of the resistors. Now I suspect that this was just residual unstable material left over from the resistor being fused.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 8 years ago in reply to mcb1

    Hi Mark,

     

    I did start at a more modest level but voltages up to 25 volts did not fuse the resistors but rather just made them hot until a burn mark could be seen on the outside of the chip. Once I got about 40 volts the chip fused quickly enough so no heat damage was noted.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 8 years ago in reply to mcb1

    Hi Mark,

     

    I did start at a more modest level but voltages up to 25 volts did not fuse the resistors but rather just made them hot until a burn mark could be seen on the outside of the chip. Once I got about 40 volts the chip fused quickly enough so no heat damage was noted.

     

    John