Passive Components
  • Technologies
  • More
Passive Components
Forum Seeking Proposals for Capacitor, Inductor or Resistor Projects
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 115 subscribers
  • Views 4200 views
  • Users 0 members are here
  • passive_featured
Related

Seeking Proposals for Capacitor, Inductor or Resistor Projects

rscasny
rscasny over 8 years ago

I am looking to sponsor passive components projects. It can be anything involving capacitors, inductors or resistors.

 

If you are instrested, please offer your project ideas in the comments below. Also, give me a rough idea of the BOM.

 

Randall

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +7
    Hi Randall, I'm planning on making a single-reference resistor standard, but I've already purchased the bits and pieces.It uses a single precision resistor - I thought it would be useful to have around…
  • fmilburn
    fmilburn over 8 years ago +5
    Using supercapacitors to store energy and power project along the lines of the Solar Bubble Blaster project that I did. The circuit consists of capacitors and diodes. If you add diodes then there are a…
  • baldengineer
    baldengineer over 8 years ago +5
    Having worked at a capacitor company, I can suggest projects like these where the caps are, relatively speaking, critical. Or at least, they are not an after-thought. Power Banks Sometimes these are called…
Parents
  • luislabmo
    luislabmo over 8 years ago

    Hi Randall,

     

    I'd love to build a custom PCB to implement a more permanent solution to a Split-core current sensor to be used in DIY projects -I used one in one of my projects. My idea is basically to work in two different approaches: with and without GND reference.

     

    The sensor probably is the main component but the rest of the components are resistors and capacitors. A burden resistor dictates the resolution of the measurements and the max current that can be sensed safely, also uses other concepts like a resistor divider.

     

    Luis

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • luislabmo
    luislabmo over 8 years ago

    Hi Randall,

     

    I'd love to build a custom PCB to implement a more permanent solution to a Split-core current sensor to be used in DIY projects -I used one in one of my projects. My idea is basically to work in two different approaches: with and without GND reference.

     

    The sensor probably is the main component but the rest of the components are resistors and capacitors. A burden resistor dictates the resolution of the measurements and the max current that can be sensed safely, also uses other concepts like a resistor divider.

     

    Luis

    • Cancel
    • Vote Up +4 Vote Down