Power & Energy
  • Technologies
  • More
Power & Energy
Blog Arcela Unveils Machine That Turns the Air into Gasoline
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 11 Jun 2025 7:27 PM Date Created
  • Views 6680 views
  • Likes 4 likes
  • Comments 6 comments
  • research
  • alternative_energy
  • fuel
  • startup
  • recycle
  • cabeatwell
  • innovation
Related
Recommended

Arcela Unveils Machine That Turns the Air into Gasoline

Catwell
Catwell
11 Jun 2025

image

Aircela demonstrated its compact machine that turns CO2 into gasoline for vehicle use. (Image Credit: Aircela)

New York-based fuels company Aircela built a compact machine capable of collecting carbon dioxide, converting it into clean, usable gasoline for vehicles without relying on fossil fuels. The refrigerator-sized device produces gas through a combination of direct air capture (DAC) and fuel synthesis, utilizing air, water, and renewable energy to accomplish this.

“We didn’t build a prototype. We built a working machine,” said Eric Dahlgren, co-founder and CEO of Aircela. “We want people to walk away knowing this isn’t too good to be true—it actually works.”

Last month, Aircela demonstrated their DAC device on a roof in New York with an audience present. The device produced gasoline on-site and in real-time. The startup says the fuel doesn’t contain any heavy metals, sulfur, and ethanol. It’s also compatible with modern car engines and infrastructure.

image

Aircela’s device successfully converted the air into gasoline. (Image Credit: Aircela)

The machine works much like a direct carbon capture facility unit, capturing CO2 from the atmosphere and turning it into gasoline. Aircela’s device has three large blue units. One is placed on the top, while the other two sit side-by-side on the bottom. These parts are responsible for air capture, water electrolysis, and fuel synthesis.

It uses a water-based solution containing potassium hydroxide to collect CO2 from the air. Air is drawn through a chamber, where it comes into contact with the liquid sorbent, allowing the potassium hydroxide to react, absorbing carbon dioxide. Electricity from renewable sources separates the water into hydrogen and oxygen. While the machine keeps the hydrogen for fuel synthesis, it releases the oxygen. The sorbent is also regenerated for reuse.

Both the hydrogen and collected CO2 are mixed in a chemical reactor and turned into methanol and then gasoline via a two-step process called methanol-to-gasoline (MTG). The fuel remains stored in the device until it’s dispensed via a gas nozzle at the back.

Overall, the device captures up to ten kg of carbon dioxide per day, producing a gallon of gasoline. It stores 17 gallons of fuel in the tank. However, with its current design and configuration, the machine won’t fill up a 20-gallon car fuel tank with gas overnight. Although the company didn’t name a price for the device, it aims to make it as affordable as possible. If the machine is mass-produced, costs can be driven down over time.

Aircela hopes to begin manufacturing by the fall, aiming to sell the product to commercial, industrial, and residential customers. “We truly believe that our approach is the fastest way to bring carbon-neutral fuels to as many people as possible, to as many places as possible, as soon as possible,” Dahlgren said.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • Fred27
    Fred27 over 1 year ago

    I don't smell gasoline. I smell a scam.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 1 year ago in reply to Fred27

    I thought the same thing at first. Blackbox technology always seems fishy. 

    However, I see how this works. I wonder if it costs as much to get the other materials to create the fuel as it would to just make it straight up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Catwell

    You could perhaps combine it with the excess off-peak energy available from existing renewables. Storing it as a liquid as opposed to batteries.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 1 year ago in reply to Catwell

    You could perhaps combine it with the excess off-peak energy available from existing renewables. Storing it as a liquid as opposed to batteries.