Power & Energy
  • Technologies
  • More
Power & Energy
Blog DiY Slip Rings: 5 Go-To Guides That Detail How To Make A Slip Ring
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
  • Author Author: c.bates
  • Date Created: 12 Sep 2016 8:52 PM Date Created
  • Views 17152 views
  • Likes 0 likes
  • Comments 1 comment
  • wind energy
  • slipring
  • How To
  • renewable_energy
  • diy
  • wireless power
  • wind turbines
  • power
Related
Recommended

DiY Slip Rings: 5 Go-To Guides That Detail How To Make A Slip Ring

c.bates
c.bates
12 Sep 2016

How do you make your own slip ring? It’s actually a surprisingly common question.

 

When you consider their multitude of uses, it’s easy to see why. For one, they help to power wind turbines, and support the ever advancing renewable energy initiatives of the future. Elsewhere, and they’re used to bring the likes of BB8 - R2D2’s heir apparent and star of The Force Awakens - to life. In fact, you’d be surprised at just how many devices and equipment - from military hardware to NASA satellites - makes use of a slip ring’s unique ability to deliver power to rotating and moving components.

 

Professional and industrial-grade slip rings are available via numerous retailers, though those looking for a slip ring solution for smaller or hobby scale projects don’t always have access to that kind of cash. Thankfully, there are numerous guides across the web that detail how to do just this, so today we’re going to round them up in the one place to make the process that much easier. Less time searching and more time making? Sounds good to me!

 

Hold Up, What Is A Slip Ring Exactly? And How Does It Work?

With a quick Google search you’ll find plenty of existing resources that dive deeper into the What, When and Where of Slip Rings. In fact, a search for ‘What are slip rings’ returns some 15,000,000 results! We’re guessing that if you’re looking for ways to build them, you probably know what you’re getting yourself into. So rather than bore you with the finer details, we’re going to bring you up to speed with a quick TL;DR:

 

At their most basic? Slip Rings are able to effectively - and efficiently - transmit electrical, data or other signals across rotating assemblies, all while effectively maintaining this connection where other stationary alternatives just couldn’t cut it. So if it moves and requires power? It’s more than likely that a slip ring is the solution.

 

The diagram below highlights how Slip Rings function in more detail:

image

 

 

Want To Make Your Own Home Made Slip Ring? Here’s How!

 

1. Home Made Slipring For Wind Turbine

Written by Chartley4 @ Instructables

The go-to source for all things hacked, homemade and DiY, Chartley4’s guide over at Instructables takes you step-by-step through the process of creating your very own slip ring for use with a wind turbine or similar device. Slip rings actually have a long-held place as a major component of commercial renewable energy projects - wind turbines included - so this project let’s you recreate this on a much smaller, but no less worthwhile scale.

 

 

2. How-To For A Slip Ring Connector Using Ball Bearings

Written by Stephan Schulz

If you like to dive into the smaller details and get your hands dirty, then Stephan’s guide is the one you’ll want to check out. Showing you how to create a slip ring using ball bearings, this guide includes a wealth of images that ensure you know what you’re doing - and why - every step of the way. Stephan’s guide came about as a way to power up fluorescent light bulbs while they were turning, which would be an impossible task without the help of a slip ring.

 

 

3. 360 Degree Range Finder Slip Ring

Written by Let’s Make Robots

Let’s Make Robots project came about as a much needed component of a project to build a 360 degree range finder. With the level of twist, turn and rotation involved in a project like this? You need a component that can handle that level of motion while still being able to deliver power effectively and reliably. Enter: Slip Rings.

 

Let’s Make Robots name also couldn’t be more apt, when you consider Slip Rings are what bring some of our most recognisable robots - whether on the silver screen, the big screen, or behind the manufacturing scenes - to life, and give them a range of flexibility and movement they wouldn’t otherwise be able to achieve. While this project can suffer from some interference and signal loss due to the parts involved, for a DiY solution it’s more than satisfactory.

 

 

4. Home Made Sliprings

Written by The Back Shed

This post from The Back Shed shows us just how easy it can be to make a slip ring for a home made wind turbines. Here, slip rings are used to address that ever present hassle of many homemade wind turbines: having to disconnect and unwind the cable time and again as it becomes tangled with use over time.

 

If you live close enough to your wind turbine? It may not be that big an issue. But if you’re unlikely to be around or situated near for prolonged periods of time, then a slip ring is your best option. And this guide is the best explanation as to both How and Why.

 

Better still? This post sets out to create a slip ring with parts readily available at any regular hardware store, which means it’s that much easier for you to pick up the parts and try this one yourself.

 

 

5. Making A Slip Ring Connector

Written by Chuck @ Fieldlines Forums

Another one for the DiY wind turbine, renewable energy crowd, Chuck over at the Fieldlines Forums shows us how he used simple, readily available plumbing parts to make his very own slip ring and brush assembly, complete with detailed pics and instructions. Not bad for a homebrew system that uses everyday components!

  • Sign in to reply
Parents
  • michaelkellett
    michaelkellett over 10 years ago

    Whilst these suggestions are interesting none of them will result in a slip ring system that is reliable and all would be unsafe for use with high powers or voltages (serious fire risk or risk of electrocution)  - wooden insulators are not a good plan.

     

    If you want slip rings that work you have to buy them, commercial products are usually the result of lots of material knowledge and testing.

     

    The last set of good instrument quality slip rings (silver brushes on silver rings, two brushes per ring) I bought was some years ago and I think they cost  perhaps £250 - now I see you can sets (not the same !!) from Amazon at prices from £5  - I doubt if they are as good but will probably work a lot better than home made ones.

     

    Steel on steel contacts or carbon brush on steel will spark a lot and wear out very quickly, ball bearings are not a good idea for the same reason.

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 10 years ago

    Whilst these suggestions are interesting none of them will result in a slip ring system that is reliable and all would be unsafe for use with high powers or voltages (serious fire risk or risk of electrocution)  - wooden insulators are not a good plan.

     

    If you want slip rings that work you have to buy them, commercial products are usually the result of lots of material knowledge and testing.

     

    The last set of good instrument quality slip rings (silver brushes on silver rings, two brushes per ring) I bought was some years ago and I think they cost  perhaps £250 - now I see you can sets (not the same !!) from Amazon at prices from £5  - I doubt if they are as good but will probably work a lot better than home made ones.

     

    Steel on steel contacts or carbon brush on steel will spark a lot and wear out very quickly, ball bearings are not a good idea for the same reason.

     

     

    MK