Power & Energy
  • Technologies
  • More
Power & Energy
Blog Fluoride Battery To Replace Lithium
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 17 Dec 2018 8:22 PM Date Created
  • Views 1586 views
  • Likes 3 likes
  • Comments 3 comments
  • research
  • on_campus
  • honda
  • battery
  • cabeatwell
  • university
  • power
Related
Recommended

Fluoride Battery To Replace Lithium

Catwell
Catwell
17 Dec 2018

image

In an attempt to find more sustainable and lasting sources of energy, scientists are developing a battery for electric vehicles that has the potential of lasting up to 10 times longer than any lithium ion battery on the market. (Image of the different components of a fluoride battery Honda)

 

Since the 1990s, the lithium battery has been the best option for portable equipment or even electric vehicles. The lithium-ion battery replaced its predecessor, the nickel battery, thanks to its lightweight and great electrochemical potential. However, with the advances in technology, the lithium-ion battery cannot keep up with the needs when it comes to mobile energy sources. Among its many drawbacks, the lithium battery ages quickly. Whether it has been used or not, the battery tends to fail after 2-3 years. The lithium battery is also expensive to make: it costs 40 percent more to make lithium than to make nickel batteries. Lithium batteries are also unsafe to operate without a protection circuit. To address those concerns and find a better alternative to lithium batteries, researchers have been experimenting with a few other metals, and they discover one that is similar to the lithium but with more potential.

 

Considered the doppelganger of lithium, fluoride is the new option to make more reliable batteries. While lithium is the most positive metal on the Mendeleev chart, fluoride is the most negatively charged. Many people know fluoride as one of the ingredients in most toothpaste. But, fluoride is actually an ionized form of fluorine, and as a negatively charged metal, it has the power to store more energy than lithium could. For that reason, a team of researchers composed of scientists from California Institute of Technology, the Honda Research Institute Inc, Lawrence Berkeley National Laboratory and the Jet Propulsion Laboratory think it can replace lithium battery in electric vehicles that travel long distances. The research team has even secured two patents in the United States for their finding about fluoride battery.

 

To make a battery, scientists need an electrolyte (preferably in liquid form) in which the ions of the base element (lithium or fluorine) will dissolve to facilitate their movements between the anode and cathode. However, the challenge was that early fluoride batteries could only work with a solid electrolyte which means that they could only be used in high temperatures. To overcome that challenge, the team of researchers turned to a new electrolyte called BTFE or Bis (2,2,2 TriFluoroEthyl) ether which will allow fluoride ions to dissolve at room temperature. BTFE is a combination of multiple groups of chemicals arranged in a way that the molecule is mostly positively charged and therefore can freely interact with fluoride’s ions. That is just the beginning of the journey to long-lasting batteries.

 

As researchers tested the new battery, they realized that the new-found electrolyte is not really stable at high voltage. So, they have been testing some other solvents like “glyme” molecules that could make the solution more stable and functioning at high voltage. During the tests, the team is also working on stabilizing the cathode and the anode of the fluoride battery. Hopefully, the world will soon enjoy the fruits of their hard work.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

 

 

  • Sign in to reply

Top Comments

  • mp2100
    mp2100 over 7 years ago in reply to Gough Lui +1
    Flourine certainly has the highest atomic electronegativity, which is great for batteries. Well, great for voltage. But flourine weighs a lot more than lithium. I mean of course, each mole of flourine…
Parents
  • DAB
    DAB over 7 years ago

    I must say, there is a predilection for using volatile elements in these new batteries.

    Lithium was bad enough, but Fluoride can be deadly in certain concentrations.

     

    It will be interesting to see what type of electrolyte they use, but I suspect that these batteries will also make the do not fly list.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to DAB

    That's basically got to do with electrochemistry, the cell voltage and energy density achievable. You'd like to have a big difference in the potentials between the elements - hence the preference towards more reactive elements. The art, as it seems, is in making it safe enough for consumer use.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 7 years ago in reply to DAB

    That's basically got to do with electrochemistry, the cell voltage and energy density achievable. You'd like to have a big difference in the potentials between the elements - hence the preference towards more reactive elements. The art, as it seems, is in making it safe enough for consumer use.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mp2100
    mp2100 over 7 years ago in reply to Gough Lui

    Flourine certainly has the highest atomic electronegativity, which is great for batteries. Well, great for voltage. But flourine weighs a lot more than lithium. I mean of course, each mole of flourine has a much higher mass. Lithium was chosen (I assume) for batteries because of its very light weight, important for batteries and density.

     

    Let’s see. Over simplified math: lithium, electronegativity 0.98, mol weight 7.  Ratio 7

    Flourine e.n. 4.0, mol wt. 19. Ratio about 5.

     

    Ok, I guess flourine wins. I’m a bit surprised. And yes, both elements on their own are very dangerous. Pyrophoric elements like lithium should not be played with. Yet I have 5 lipo batteries on my bench. Flourine is toxic, will attack your bones.  Let’s see how the new batteries are developed.