Power & Energy
  • Technologies
  • More
Power & Energy
Blog How to kill a battery tester
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: cookmesomekai
  • Date Created: 27 May 2020 12:30 PM Date Created
  • Views 2538 views
  • Likes 7 likes
  • Comments 5 comments
  • bt3554
  • hioki
  • littlefuse
  • battery tester
Related
Recommended

How to kill a battery tester

cookmesomekai
cookmesomekai
27 May 2020

A very popular HIOKI instrument is the BT3554 battery tester. It's a portable instrument designed primarily for maintenance purposes with voltage ranges up to 60V.

image

Of course the BT3554 won't blow up when you accidentially apply 61V to it instead of the maximum 60V. In fact there are not many service cases for the BT3554 at all. However, about 9 out of 10 BT3554 that arrive in HIOKI's service department in Frankfurt, Germany are identified to have suffered some sort of over-voltage. The majority of those cases could have been prevented simply by replacing the original fuse in the BT3554 with the exact same type of fuse once it blew - which typically happens after the BT3554 has been subjected to some sort of overvoltage.

 

So the easiest way to kill a BT3554 battery tester is by replacing a blown fuse with something else and then have another overvoltage situation occur. To be fair, replacing a fuse with a different type or value to the one specified would probably damage all kind of T&M instruments in an overvoltage situation and not only this specific battery tester.

image

The correct fuse for the BT3554 is a fast acting 630mA ceramic fuse (indicated by the "H" next to the capacity). Ceramic fuses have much higher breaking capacities than normal glass fuses. If a fuse needs replacing in the field to be able to continue with a job then it is typically more likely that there is a glass fuse flying around somewhere rather than a ceramic one (there is a spare fuse coming with every BT3554, by the way). However, replacing a ceramic fuse with a glass fuse (and even worse with any available value) makes it more likely that the instrument gets damaged when subjected to an overvoltage in the future. That might happen months later when it has been long forgotten that the glass fuse found in the van at the time was only to be used as a quick fix with the firm plan of ordering the right one once back at the base. But as you can see the required fuse in the BT3554 is nothing special but a standard ceramic fuse which is available from the same manufacturer (Littlefuse) at Farnell (SKU #1354537). Get some of them, put them in the BT3554 box and you can significantly reduce the risk of a repair case.

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 6 years ago +2
    Great advice regardless of the brand of your meter. John
  • colporteur
    colporteur over 6 years ago +1
    I took a moment to read about ceramic and glass fuses. Who knew? I didn't. Amperage and voltage is all I looked at when digging through the bottom of the tool box to find a fuse. Thank you for the insightful…
  • Gough Lui
    Gough Lui over 6 years ago in reply to colporteur +1
    There's plenty to worry about with fuses if you delve into the subject. For example - the fusing characteristic comes in a number of different ratings - the more common is F for "fast blow" and T for …
Parents
  • three-phase
    three-phase over 6 years ago

    This is quite intriguing to me, is there any more information that can be released as to the industry sector these instruments with the incorrect fuse came from? I know in my industry there is an awful lot of effort into ensuring that electricians utilise the correct fuse in their instrument and test leads, should they need to be replaced.

     

    Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 6 years ago

    This is quite intriguing to me, is there any more information that can be released as to the industry sector these instruments with the incorrect fuse came from? I know in my industry there is an awful lot of effort into ensuring that electricians utilise the correct fuse in their instrument and test leads, should they need to be replaced.

     

    Kind regards