Power & Energy
  • Technologies
  • More
Power & Energy
Blog Japan builds world's largest floating solar power station
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 24 Jun 2015 5:31 PM Date Created
  • Views 2940 views
  • Likes 2 likes
  • Comments 6 comments
  • clean
  • green
  • japan
  • cabeatwell
  • floating_solar
  • solar
  • larges_floating_solar
  • innovation
Related
Recommended

Japan builds world's largest floating solar power station

Catwell
Catwell
24 Jun 2015

image

9,000 solar panels sitting on top of the water to power surrounding homes near Japan's Yamakura Dam (via Kyocera & JapanTimes)


Conserving power and energy is still a big issue people around the world are trying to find solutions to. Most turn to solar power, which can power a number of different things, but the panels are usually built into or on top of the object it's trying to run. Japan has a different technique when it comes to solar power.

 

The Kyocera Corporation recently revealed the world's biggest floating solar power station on a reservoir of Japan's Yamakura Dam in Chiba prefecture, which uses 9,000 waterproof panels that sit right on top of the water's surface. With an estimated production of 2,680 megawatt-hours per year, this massive power station has the capacity to power 820 households. The station measures 333 meters in length and 77 meters in width making it around 25,000 square miles. It will also decrease nearly 8,000 tons of carbon dioxide emissions per year. This is only the first step in a larger project to revealed near Tokyo that will be able to power about 5,000 homes next year. Right now, the energy it produces will be sold to Kansai Electric Power in Osaka for about 96 million Yen ($780,000).

 

It seems unconventional to build these solar panels on top of water, but a lot of benefits come with it. Since the panels are on water, it frees up the surrounding land for agricultural use, conservation, and other development. They'll also help prevent excess heat in the panels making them 11 percent more efficient than land based ones. The shade provided by the panels will also prevent excess algae growth and evaporation. The station is also very sturdy since it is capable of withstanding winds up to 118 miles per hour and are even earthquake proof. But the floating station also presents some new issues.

 

Since the panels sit directly on top of the water, everything needs to be waterproofed, such as the wiring. Regulations on water quality also have to be taken into consideration since this artificial object is sitting in a natural resource. Ichiro Ikedea, the general manager of Kyocera's solar energy marketing division, responded to the possible problem by saying “That is one reason we chose Ciel et Terre's floating platforms, which are 100 percent recyclable and made of high-density polyethylene that can withstand ultraviolet rays and corrosion.”

 

Still, the floating water station in a step in the right direction when it comes to Japan's goal of entirely switching to renewable energy sources by 2040. Japan isn't the only country to get on board with floating solar panels. India, Australia, Great Britain, Brazil, and Sonoma County, California are currently using similar models in hopes of using an alternative energy source.

 

C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • johnbeetem
    johnbeetem over 11 years ago in reply to clem57 +1
    Clem Martins wrote: Really? I never thought about the heat build up in solar panels... Solar cells aren't very efficient. According to Wikipedia , typical commercial panels are 14%-19% efficient…
  • PaulMakesThings
    PaulMakesThings over 11 years ago +1
    Pretty cool, your typo got me for a second though " 25,000 square miles" that would be big enough to power the whole US at least. It would cover the entirety of some of the smaller eastern states. It would…
  • e14 Contributor
    e14 Contributor over 11 years ago

    Floating Solar Power Systems are wonderful Ideas.

    You can see all the advantages of this product on the water on this site:

           http://www.ciel-et-terre.net/hydrelio-floating-solar-system/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • PaulMakesThings
    PaulMakesThings over 11 years ago

    Pretty cool, your typo got me for a second though "25,000 square miles" that would be big enough to power the whole US at least. It would cover the entirety of some of the smaller eastern states. It would be cool if they did build one that big.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to clem57

    I never thought about the heat build up in solar panels...

    If we paint you black and leave you out in the sun ...will that work image

     

    I didn't really think the efficiency of a device designed to capture that same energy would be less either ... but there you go.

     

    I like the inefficiencies in manufacturing and waste that this 'green technology' brings ...

     

    The Australians have some other LSA where they stick a lens in front ... it still has some issues, and maybe it's better/worse to manufacture.

    It is not as efficient in hazy conditions due to the light spectrum and the lens ....

     

     

    Fundamentally the use of bodies of water is a great idea ...

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to clem57

    Clem Martins wrote:

     

    Really? I never thought about the heat build up in solar panels...

    Solar cells aren't very efficient.  According to Wikipedia, typical commercial panels are 14%-19% efficient.  You can get 30%-44% at much higher expense.

     

    So the rest of that solar energy heats those nice black panels.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to mcb1

    Really? I never thought about the heat build up in solar panels...

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>