Power & Energy
  • Technologies
  • More
Power & Energy
Blog LED Filament Light Bulbs
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
EMI-Reduction-Techniques
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gsimerlink
  • Date Created: 13 Jul 2015 8:16 PM Date Created
  • Views 712 views
  • Likes 0 likes
  • Comments 0 comments
  • lighting
  • led
  • efficiency
  • energy
Related
Recommended

LED Filament Light Bulbs

gsimerlink
gsimerlink
13 Jul 2015


image

Now Available! An expanding line of Pro Elec LED Filament Light Bulbs which mimic incandescent bulbs with their classic shape and a similar looking filament. If you like the look and feel of classic incandescent light bulbs then you will love these LED's which are virtually indistinguishable to clear incandescent bulbs when lit! Currently we have LED light bulbs available in the classic A19 shape and the popular candelabra style.


Available Bulbs:
25-7410 - 2 Watt Dimmable LED Filament Candelabra Bulb
25-7415 - 4 Watt Non-Dimmable LED Filament Candelabra Bulb
25-7420 - 5 Watt Dimmable LED Filament A19 Standard Bulb
25-7425 - 4 Watt Non-Dimmable LED Filament A19 Standard Bulb
25-7430 - 7 Watt Non-Dimmable LED Filament A19 Standard Bulb


image

 

Reasons to Buy LED Light Bulbs

There are several great reasons to replace your current light bulbs with high efficiency LED light bulbs: they save you money on your electric bill, have superior light quality, cause less impact on the environment plus you only need to replace them once every decade instead of several times a year.


Cost Comparison Between LED, CFL and Incandescent Light Bulbs

 

LEDCFLIncandescent
Light Bulb Projected Life Span25,000 Hours10,000 Hours1,200 Hours
Cost Per Bulb$9.99$6.49$1.25
KWh of electricity used over 25,000 hours2503501500
Cost of Electricity (@ 0.10per KWh)$25$35$150
Bulbs Needed for 25k Hours of Use1321
Equivalent 25,000 Hours Bulb Expense$9.99$19.47$52.50
Total Cost for 25,000 Hours$34.99$54.47$176.25


As you can see LEDs last a long time, virtually forever in comparison to incandescents. Plus LEDs don’t burn out or suddenly stop working like other types of bulbs. Instead, LEDs produce less light over a period of time. This is known as “lumen depreciation”. In other words, the amount of LED light produced decreases over a period of time, and so does color accuracy. Therefore, the LED’s lifetime is based on a prediction of when the light output will decrease by 30 percent.

Energy Star calculates that switching just one bulb from incandescent to Energy Star will reduce energy consumption between 70 to 90 percent and save $30 to $80 on utility bills over the lifetime of the bulb.


Equivalent Wattages and Light Output of LED, CFL and Incandescent Bulbs

 

Light OutputLEDCFLIncandescent
LumensWattsWattsWatts
4504-58-1240
750-9006-813-1870
1100-13009-1318-2275-100
1600-180016-2023-30100
2600-280025-2830-55150

* Chart Courtesy of Eartheasy.com


LED technology converts 95 percent of the energy to light and only 5 percent is wasted as heat. Incandescents are pretty much the opposite. They convert only 10 percent of the energy into light, while 90 percent is wasted as heat.


Comparing Features of LED, CFL and Incandescent Bulbs

 

LEDCFLIncandescent
Frequent On/Off CyclingNo EffectShortens LifespanMinimal Effect
Turns on InstantlyYesSlight DelayYes
Heat EmittedLow (3 btu's/hr)Med (15 btu's/hr)High (85 btu's/hr)
Sensitivity to High TemperaturesSomeYesNo
Sensitivity to Low TemperaturesNoYesNo
Sensitivity to HumidityNoYesSome
Hazardous MaterialsNone5 mg Mercury/BulbNone
Replacement Frequency (25k Hours)1321

* Chart Courtesy of Eartheasy.com


Light Bulb Uses Based on Color

 

image

Our line of LED Light Bulbs all fall into the 2700K color range, which is a great match for standard incandescent bulbs. Another great use for LED bulbs is for wine storage because they emit very little heat. Too much heat can cause a temperature imbalance and affect the quality of the wine.


MCM Electronics is a sister company of element14 and part of Premier Farnell