Power & Energy
  • Technologies
  • More
Power & Energy
Blog Microsoft Surface Book 2 Power Supply Teardown
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 27 Feb 2024 2:38 PM Date Created
  • Views 9173 views
  • Likes 10 likes
  • Comments 15 comments
  • laptop charger
  • power supply
  • psu
  • ac-dc supply
  • teardown
Related
Recommended

Microsoft Surface Book 2 Power Supply Teardown

shabaz
shabaz
27 Feb 2024

Table of Contents

  • Introduction
  • Removing the Case and Shielding
  • What Parts are Used?

Introduction

I’ve got through a lot of model “1798” power supplies! They come with Surface laptops, and they don’t seem to last much beyond a couple of years.

image

(image source: Microsoft website)

Just out of curiosity, here is a teardown of one, so we can see how it operates. Note: it’s not possible to repair these, it is a destructive teardown because the plastic case is welded shut, and there are metal shields and an insulating cement which needs to be chipped away in places.

I was wondering why these power bricks cost £100. After tearing it down, now I realize why, and I don’t feel so bad having to buy another one. But first, for a comparison, here’s what a cheap clone can look like on the inside, courtesy of Big Clive:

image 

(Image source: Big Clive video)


It’s worth watching the Big Clive video, to see how such a charger can destroy a laptop and external monitor!

Removing the Case and Shielding

The case needs to be milled off. It’s not going to come apart anytime soon even with a hacksaw, without a lot of damage. Milling reduces the chances of wrecking it further. Inside, the power supply has a copper shield surrounding it. I liked that the mains connector, and the USB connector, are “floating” so that they do not cause stress on the PCB when plugged/unplugged.

Notice that the main charging lead has four connections, not just two! The two thin wires detect when the magnetic connector is fully attached, and then turn on the supply. The cheap clone chargers omit this, and (presumably) cause arcing and damage to the laptop.

image

The magnetic connector:

image


Another photo showing lots of copper shielding.

image


I snipped off the shielding connections, and then bent off the heatshinks although I could have unsoldered them the PCB. Parts are attached to the heatsinks using thermally conductive adhesive tape, and they came off fine.

image

What Parts are Used?

There’s a lot of wound components, so that’s going to be a significant part of the expense. The entire supply is custom (manufactured by Chicony).

Most of the MOSFETs are from Infineon, and the power factor correction (PFC) and power supply controller IC are from NXP.

The bridge rectifier is a Diodes Inc GBP808N, capable of 8A with a heatsink (the parts on the side of the board were connected to a heatsink plate, which I've removed and is not shown). Power factor correction uses the NXP TEA19162T, along with a ST STTH5L06 600V 5A ultrafast rectifier, and IPD60R380P6 Infineon CoolMOS P6 N-channel MOSFET.

image

A view of the mains filter portion:

image


Power factor correction (PFC) chip TEA19162T was buried under the white stuff:

image

The STTH5L06 rectifier:

image

An NXP TEA19161T (the 16-pin SOIC in the photo below) is used as the switching controller for a resonant supply.

image

Close-up view of that area:

image


The transformer looks custom, and is pretty compact (about 30x30x18mm) considering it needs to support just over 100W.

Here's the STFH24N60M2 N-ch 600V MOSFET used for the resonant converter:

image

On the DC output side, a MPS MP6922 MOSFET controller (the 8-pin SOIC in the photo below) is used, to control a couple of AOL1240 N-channel MOSFETs, to perform synchronous rectification (i.e. used as active diodes) for higher efficiency.

image



MOSFETs excavated from the white stuff on the other side:

image

Opto-isolators:

image



There is a SSOP-14 part labelled SH3H0003S that I couldn’t find any information for, but I believe it is related to the USB power output connector (the power brick has a separate USB output intended for charging phones and so on).

image



Underside of the USB board:

image



There’s also an INA213 chip and a sense resistor, so current is actually monitored, and there’s a MOSFET to switch the supply on or off, presumably under control of the two thin wires within the DC output cable.


All-in-all, I can see that the power supply probably is worth the £100. It’s just a pity it doesn’t last all that long. However, on the plus side, there’s a newer compatible model 1932, and that may last longer.

Thanks for reading!

  • Sign in to reply
  • fyaocn
    fyaocn over 2 years ago in reply to shabaz

    Indeed, 65W PD can drive Surface book 2 in normal no-GPU (need BIOS setting) operation and slow charging. 

    But there is still unamed PD cheating adapter rating 15V-6.8A(102W max) available, and 130W PD charger need unlock the 15V output unless PPS is supported. So, it is not recommended.

    I have thrown away my original 135W Lenovo power adapter,  since Lenovo provides alternative Legion PD charger choice. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to fyaocn

    That's a good tip for a lot of the Surface family. My Surface Book 2 needs 100W+ (the larger screen version with dual GPU, apparently it can draw up to 105W) so it cannot run indefinitely on USB-C charging (without slowing the processor, or draining the battery simultaneously), so I had no choice : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fyaocn
    fyaocn over 2 years ago

    In fact, no need for another power supply from Microsoft, just select on Fast Charge Power Delivery (PD) adapter for surface., plus one good 65W USB PD charger. More portable.

    The PD adapter can cheat the USB charger for require power supply. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to e14phil

    Definitely a weird connector! I blame Apple for pioneering poor strain relief and then others blindly copy : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 2 years ago

    These power supplies are connectors are such a pain. My partner had two Microsoft Surfaces and specifically moved platform because of how many replacement chargers she has had to buy.  She had strain relief fail a few times and the charger its self other times. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>