Power & Energy
  • Technologies
  • More
Power & Energy
Blog NYIT professor looks to send wireless power at long distances using lasers and balloons
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 20 Dec 2013 7:53 PM Date Created
  • Views 1168 views
  • Likes 0 likes
  • Comments 2 comments
  • defense
  • military
  • power_management
  • aerostat
  • cabeatwell
  • wireless
  • power
Related
Recommended

NYIT professor looks to send wireless power at long distances using lasers and balloons

Catwell
Catwell
20 Dec 2013

imageimage

(Right) Aerostat depiction. (via US Military)


The idea of sending power wirelessly over considerable distances has been around since Nikola Tesla demonstrated that ability using his Tesla Coils back in the late 1880’s and early 1900’s. Since that time, scientists have designed alternative ways to deliver power without the use of wires, however the distances are on relatively small-scale levels (think feet rather than miles). Now a professor at the New York Institute of Technology is looking to send significant levels of power over hundreds of miles using military-grade balloons (known as aerostats) and lasers. The military’s aerostat balloons have been in use for quite some time now on the battlefields of Iraq and Afghanistan for surveillance, so those balloons are ideal as they are both robust in nature and can carry fairly heavy loads. Professor Stephen Blank’s (NYIT’s Engineering and Computer Sciences department) system would use a laser, beamed through a fiber-optic cable up to the aerostat positioned above the laser’s source. The laser would then be beamed over to a distant balloon, where it is received and then converted over to electrical energy (hundreds of kilowatts) and sent back to earth via the balloons tether, where it can then be utilized. Professor Blank states that the first initial use of this system would be used to get power to disaster zones, such as the Philippines that was recently ravaged by typhoon Haiyan. Essentially power could be acquired from an aircraft carrier’s nuclear generator stationed off the coast of disaster zones and send that emergency power to where it’s needed, such as hospitals and trauma centers. The end-goal for the technology however, is for use as a space-based solar power collector, whose energy is then beamed back to earth via lasers.




C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 12 years ago +1
    This sounds to me as if the professor had slightly overdone it with the mulled wine at the end of term Christmas party ! Obvious problems are: Several very lossy power conversions. Aiming the laser from…
Parents
  • michaelkellett
    michaelkellett over 12 years ago

    This sounds to me as if the professor had slightly overdone it with the mulled wine at the end of term Christmas party !

    Obvious problems are:

    Several very lossy power conversions.

    Aiming the laser from one ballon to another.

    Loss of power in air (needs dense atmosphere to float balloons so can't go very high).

     

    etc etc etc.

     

    I really do think that it's bad form for University engineering departments to put ot these silly press releases without any numbers ot back them up - if there are no numbers (which idealy should come from actual measurements but simulation will do) then it isn't engineering.

     

    The left hand picture seems to be of some hand held laser pointers and the right hand a stock picture of some military comms/fire control stuff.

     

    Thanks for the reference though, it's given me the chance to get the rant above off my chest.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to michaelkellett

    Hi Mike,

     

    I had the same thought.  Yes you can do it, but your will only recover about 5% of your input power at your download point.

    You would be better off connecting a diesel powered generator to the balloon and place it in the affected area.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago in reply to michaelkellett

    Hi Mike,

     

    I had the same thought.  Yes you can do it, but your will only recover about 5% of your input power at your download point.

    You would be better off connecting a diesel powered generator to the balloon and place it in the affected area.

     

    DAB