Power & Energy
  • Technologies
  • More
Power & Energy
Blog Researchers Developed a Tent That Produces Electricity from Mechanical Motion
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
  • Author Author: Catwell
  • Date Created: 23 Nov 2026 10:00 AM Date Created
  • Views 8 views
  • Likes 1 like
  • Comments 0 comments
  • hmi
  • off the grid
  • energy_harvesting
  • camping
  • power
  • energy
  • magnetomechanical
  • magnetoelastic
  • innovation
Related
Recommended

Researchers Developed a Tent That Produces Electricity from Mechanical Motion

Catwell
Catwell
23 Nov 2026

image

(Image Credit: Jesse Gardner/Unsplash)    

Researchers at the University of California, Los Angeles, developed a magnetoelastic tent that produces power from mechanical motion. Unhoused and off-grid communities could use this smart tent, which may power small electronics like communication devices and lights.

The magnetoelastic textiles have two layers. For starters, the magnetomechanical coupling layer has micromagnets in a soft matrix. So, bending or compressing the fabric forces the particles to change position or orientation. And that alters the local magnetic field. Then, a magnetic induction layer of conductive fibers turns that changing flux into current via electromagnetic induction.

Each part of the tent captures energy available in it. The floor uses alternating ribbons of magnetoelastic material and fabric. Biomechanical inputs like footsteps and body movement get harvested from it. The roof consists of layers of conductive fibers and magnetoelastic film. This captures wind- and rain-driven flexing. Weaving patterns, like plain, twill, and satin, were optimized along with layer stacking and the number of conductive-fiber turns. A three-layer stack exhibited good performance as the middle layer was rotated 90 degrees from the top and bottom layers. This increased contact with the induction layer. A transformer and bridge rectifier convert the output into DC, which powers small devices.

A 20-by-20-centimeter textile provided up to 0.094 mW of instantaneous power (optimal load resistance of 100 Ohms). It remained stable over 12,000 continuous cycles at 5 hertz and 4mm displacement.

Testing for over 2,400 seconds harvests 0.191 Joules. If someone gently tapped with their hand, the tent would charge a 0.22 mF capacitor to 5.80 V in just 1.5 seconds. A 680-mf capacitor reached 5V and stored 8.5 millijoules. Rain generated a stronger electrical response compared to artificial wind. That’s because droplet impacts formed sharper, more impulsive deformation.

The tent doesn’t provide continuous high-power electricity. In the team’s demonstrations, the system powered an LED and a digital thermometer. The fabric runs at 1-10 Hz frequencies, similar to human motion rhythm. It’s also waterproof, lightweight, and recyclable.

However, scale is the key limitation, as 0.094 milliwatts is insufficient for household energy needs. Output could be increased in the future by making the active textile bigger or connecting multiple units. Better capacitors, rechargeable batteries, and voltage-regulation electronics could make the captured energy more useful.

Have a story tip? Message me here at element14.