Power & Energy
  • Technologies
  • More
Power & Energy
Blog Rexi and GENNY create drinkable water from the air
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 16 Jan 2020 6:43 PM Date Created
  • Views 3073 views
  • Likes 5 likes
  • Comments 5 comments
  • ces2020
  • hmi
  • water
  • cabeatwell
  • ces
  • solar
  • innovation
Related
Recommended

Rexi and GENNY create drinkable water from the air

Catwell
Catwell
16 Jan 2020

image

Zero Mass Water unveiled their new Rexi Source hydropanel at CES 2020. The device promises to produce drinkable water out of the air. (Image Credit: Zero Mass Water)

 

At CES 2020, Zero Mass Water, a startup based in Arizona, unveiled its Rexi Source hydropanel, a panel that looks similar to a solar roof panel, except it doesn’t harness energy from the sun, but instead creates water from the air. This new device could help create drinking water where it’s not accessible or unsafe in communities around the world. The panel costs $2,500, and that excludes installation prices, which is estimated to cost another $1,000.

 

The company’s hydropanels use solar power to extract moisture from the air, absorbs it into hygroscopic material and condenses it into water. It also comes equipped with sensors and a cellular connection that allows the owner to check up on the status of the panel. It can also connect to the Zero Mass’ network to share data analysis and to detect any faults in the panel.

 

Once the water is created, minerals like calcium and magnesium are added to make it pure. Afterward, the water gets pumped to the owner’s house, skipping water utilities, so there’s no chance of contamination. There isn’t much maintenance to worry about either since the air filter will only need to be replaced once a year and the mineral cartridge every five years.

 

There is only about a gallon of water produced per day by the hydropanel, so it’s not a freshwater replacement. Zero Mass markets the Rexi as a way to take control of drinkable water while making it risk-free.

 

However, the hydropanel doesn’t operate in cold climates. When the temperature gets too cold, the panel goes into the ‘hibernate’ mode, which prevents damage to the panel, making it impossible to get water during the winter.

 

Watergen, a Water tech company, was also involved in CES 2020, unveiled the solar-powered GENNY, a newer version of its moisture-based water system. The new GENNY costs between $5,000 - $8,000, with all expenses, including shipping and installation accounted for. A launch date has yet to be announced.

 

The current GENNY system acts as a dehumidifier, drawing in moist air through a filter in the back of the device, cleaning it and dispensing it out the front. Like most water coolers, it requires a wall outlet to function. It can dispense up to 13 liters of water per day with 9 kWh of energy and can function in temperatures ranging from 15-40 degrees Celsius with over 25% of relative humidity. 

 

The new GENNY model runs on the same technology but doesn’t need a wall outlet to function. Instead, it relies on four massive solar panels that ship with the device.  It can serve people who live off the grid and could be useful for those who need drinking water in less-developed countries or in a crisis zone.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 6 years ago +3
    A comparable development, viewed from practical point of view: www.youtube.com/watch
  • dubbie
    dubbie over 6 years ago +1
    Well any de-humidifier produces water from air, quite a lot of water depending on how humid or damp the air is. I guess if the water is purified properly it should be perfectly drinkable. Not sure how…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to dubbie +1
    The locations where de-humifiers collect some water aren’t locations with water shortage. Check that first video for the calculations..
Parents
  • dubbie
    dubbie over 6 years ago

    Well any de-humidifier produces water from air, quite a lot of water depending on how humid or damp the air is. I guess if the water is purified properly it should be perfectly drinkable. Not sure how they stop the mould growing though - there's always mould when there's water. I wouldn't describe it was free, you still have to put energy in to get the water out but in some circumstances it is probably a good product.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to dubbie

    The locations where de-humifiers collect some water aren’t locations with water shortage. Check that first video for the calculations..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to dubbie

    The locations where de-humifiers collect some water aren’t locations with water shortage. Check that first video for the calculations..