Power & Energy
  • Technologies
  • More
Power & Energy
Blog The Energy Efficiency Manifesto
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 12 May 2016 3:11 PM Date Created
  • Views 2149 views
  • Likes 7 likes
  • Comments 11 comments
  • manifesto
  • energy efficiency
Related
Recommended

The Energy Efficiency Manifesto

spannerspencer
spannerspencer
12 May 2016

Around the element14 offices, we've been chatting a lot lately about energy efficiency and this has prompted us to begin collecting our thoughts on the subject. As always, an important part of this process is gaining your opinions on the matter to clear up some of the ambiguity surrounding what energy efficiency actually means to us all. Ultimately, this'll help guide the direction of new content, campaigns or programs we'll be initiating here on the Community that are focused on the subject.

 

So, What Do We Mean by "Energy Efficiency"?

The two words aren't difficult to decipher, so the phrase itself is pretty self-explanatory. So any ambiguity around energy efficiency, therefore, isn't its definition so much as uncovering its clear differentiation from similar subjects. Primarily sustainable energy, and renewable energy, but also topics like power management and energy harvesting.

 

These are all closely related, but they're in no way the same thing. I did have a long and (obviously) highly entertaining and insightful blog post written out here, when I realised that a Venn diagram would be... well, more efficient.

image

What do you think? Do you agree with it?

 

I felt it would be equally useful to really drill down into the concept of energy efficiency, and try and give it something of a short, precise manifesto. A simple doctrine that we can use here at element14 as an easy and, yes, efficient measuring stick to hold up against a project, an idea, a campaign, a solution or a problem and instantly be able to tell if it falls within the exciting dominion of energy efficiency.

 

This is a starting point, and I'd like your input and assistance in refining the following treatise on energy efficiency (please put your thoughts in the comments section at the bottom).

 

 

 

 

imageTHE element14 ENERGY EFFICIENCY MANIFESTOimage

 

 

Energy efficiency is the practice of reducing power requirements while retaining the same function, service or operation.

 

 

Although it's closely related to, and is likely to play a part in the following practices, energy efficiency should not be confused with:

  • The conservation of energy, as this also includes the reduction, refinement or elimination of the function or service that's being powered.
  • The sustainability of an energy source, as this does not necessarily impact the reduction of energy required by the function or service.
  • The management or delivery of energy, as the primary purpose of this practice is indifferent to the efficient use of the supplied power.

 

Energy efficiency should be approached as a solution when one or more of the following, primary benefits are sought:

  • Reduction in the financial costs, work and effort of providing a function's or service's operation.
  • Sustaining a function's or service's ongoing operation in situations where limited power is available.
  • Easing the strain on power generation and reducing the harmful or costly results of energy production.

 

Example: Automatically (or manually) turning a light off is not energy efficiency; this is energy conservation as you also eliminate the service.

Replacing an incandescent light bulb with a low energy LED lamp is energy efficient, as it retains the same level of service (the luminance), but requires less power to provide it.

 

 

Your thoughts, refinements and feedback below, please!

  • Sign in to reply

Top Comments

  • spannerspencer
    spannerspencer over 10 years ago in reply to clem57 +2
    Oh, I like that phrase! Energy efficiency and renewable energy are said to be the twin pillars of sustainable energy policy. I might have to steal that
  • dougw
    dougw over 10 years ago +2
    One other motive for efficiency is weight and size reduction - very important when wearable electronics are involved. Carrying huge batteries is very clearly undesirable and more efficient electrical systems…
  • mcb1
    mcb1 over 10 years ago in reply to jkutzsch +2
    when I discuss the benefits of purchasing a Tesla automobile with the wife I have an electric car ... well actually all mine are electric. They have a key which turns on the power to the ignition system…
Parents
  • jkutzsch
    jkutzsch over 10 years ago

    I like it!

     

    One of the things that was discussed a lot with us during the purchase of our home this last month was Return On Investment for Energy Efficiency upgrades.

     

    If you are a U.S. Veteran and you are applying for a Veteran Home Loan you can also apply to have money set aside for Energy Efficiency upgrades.  They require a lot of paperwork showing exactly how much the existing costs of energy use is, how much the expected savings from the new upgrade will provide, and how much the actual upgrades cost.  Then the math is applied to see if you are truly saving money by upgrading.

     

    For example we looked into Solar Panel upgrades and Solar Water heating.  Compared to the money that is spent on normal electricity connections we could have panels installed that would fully cover our energy needs with surplus for growth.  The monthly payments for the panels would be the same as the monthly electricity bill so it would balance out.  With the fact that it is expected that the Energy companies will continue to raise their prices but my Solar Panel monthly bill would stay the same, after a couple of years we would be paying less then we would be staying connected to the standard utilities.  This would be a good Energy upgrade, alas it was also a large enough investment that the loan officers wouldn't look at it.  :-(

     

    The Solar Water Heater though would cost more then we would save over time from our Natural Gas Water Heater that we will be going to.  Although to be fair, currently it is on Propane and with Propane, Solar is better.  So while purchasing a Solar Water Heater would be more Energy Efficient and also Sustainable, the costs incurred would not be substantial enough to allow for the upgrade over Natural Gas.

     

    Since the cap on the loan was so low we ended up ordering new energy star rated windows and will be having them installed.

     

    ROI is a big factor that comes up when I discuss the benefits of purchasing a Tesla automobile with the wife to save on gas.  :-)  Until they expand their battery range I will be unable to take that upgrade either.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 10 years ago in reply to jkutzsch

    ...purchasing a Tesla automobile with the wife to save on gas.

     

    At current pricing (>$100k CAD here!) it's still mainly a luxury car. compared to a nice gasoline car, that extra $75k buys a LOT of gas!

     

    Even the more affordable cars like the Nissan Leaf and Mitsubishi iMiev include a hefty added cost over comparable non-electrics, but at least those are within range of a possible ROI.

     

    I'm hoping the $35k models planned for 2 years from now will spark some competition and bring prices down image

     

    That said, if any of my apps go viral I'll buy a Tesla just for the cool factor image

     

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 10 years ago in reply to jkutzsch

    ...purchasing a Tesla automobile with the wife to save on gas.

     

    At current pricing (>$100k CAD here!) it's still mainly a luxury car. compared to a nice gasoline car, that extra $75k buys a LOT of gas!

     

    Even the more affordable cars like the Nissan Leaf and Mitsubishi iMiev include a hefty added cost over comparable non-electrics, but at least those are within range of a possible ROI.

     

    I'm hoping the $35k models planned for 2 years from now will spark some competition and bring prices down image

     

    That said, if any of my apps go viral I'll buy a Tesla just for the cool factor image

     

    -Nico