Power & Energy
  • Technologies
  • More
Power & Energy
Blog USB-PD - Explaining the Power Standard in the Raspberry Pi 5
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dychen
  • Date Created: 29 Sep 2023 7:49 PM Date Created
  • Views 36267 views
  • Likes 8 likes
  • Comments 22 comments
  • charging
  • power delivery
  • fast charging
  • pd
  • usb type-c
  • usb-c
  • raspberry pi 5
  • raspberry pi
  • usb-pd
  • compatibility
  • charger
  • bidirectional charging
Related
Recommended

USB-PD - Explaining the Power Standard in the Raspberry Pi 5

dychen
dychen
29 Sep 2023

In our ever-connected world, a universal charging solution has become a necessity. Imagine being able to charge your smartphone, laptop, tablet, and even some appliances with a single cable and charger. That's where USB Power Delivery (USB-PD) steps in – a game-changing technology that's reshaping the way we power and charge our devices.

Before we jump into the details of USB-PD, let's look at the state of charging technology a few years ago. You probably have a drawer filled with various chargers, each with a different connector and power rating. Charging your smartphone with your laptop charger? Forget about it. Charging your tablet with your camera charger? Not a chance. It was a world of tangled cables and compatibility issues.

What is USB-PD?

USB-PD, short for USB Power Delivery, is a standardized protocol and specification designed to deliver higher levels of power and greater flexibility in charging and powering electronic devices. In simpler terms, it's a universal power solution that eliminates the need for multiple chargers and cables.

USB-PD Power Range

Figure 1: USB-PD Power Range (Source: CUI, Inc.)

Remember the frustration of hunting for the right charger or cable when you needed to charge your various gadgets? With USB-PD, you can charge a wide range of devices, from smartphones and laptops to monitors and small appliances, all using a single cable and charger. No more clutter of tangled cables or confusion over which charger goes with what device.

Key Features of USB Power Delivery:

Increased Power Levels: USB-PD supports power levels from 5W to 100W or more. This means it can handle the charging needs of not just your smartphone, but also power-hungry devices like laptops and smaller household appliances.

Bi-Directional Power Flow: USB-PD allows power to flow in both directions. This means your laptop can charge your smartphone, or two laptops can share power between each other.

Negotiation of Power Levels: USB-PD devices communicate with each other to determine the right power level and voltage needed for charging or powering. This ensures safe and efficient power delivery based on the connected devices' capabilities.

Variable Voltage and Current: USB-PD can deliver power at various voltage and current levels, adapting to the specific requirements of the device. This helps prevent overcharging and ensures that your devices get the right amount of power.

USB Type-C Connector: USB-PD is often associated with the USB Type-C connector. This reversible and versatile connector can handle higher power levels and data transfer, making it a perfect match for USB-PD technology.

Fast Charging: USB-PD supports fast-charging capabilities, ensuring your devices charge quickly and efficiently.

Universal Compatibility: One of USB-PD's primary goals is universal compatibility. It's supported by numerous device manufacturers, making it easier for you to use a single charger or power bank for all your devices.

Does the Raspberry Pi 5 Support USB-PD?

Raspberry Pi 5 USB-PD Official ChargerYes! A new feature on the Pi 5 is support for USB-PD. There's a new official power supply for the Pi5: the 27W USB-C PD Power Supply . Normally, the total power available at the Pi 5's four USB ports is limited to a nominal 600mA. When the new power supply is detected, that increases to 1.6A, letting the Raspberry Pi 5 power a much wider range of peripherals.

Embracing the Future of Charging

USB-PD has quickly become a standard in the tech industry, simplifying power management and improving the user experience when it comes to charging and powering electronic devices. With its ability to deliver higher power, fast-charging capabilities, and universal compatibility, it's a technology that's transforming the way we stay connected.

For more information on USB-C and USB-PD, check out Tech Spotlight: What's Coming Up in the Changing World of USB?

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 2 years ago +1
    "...is a standardized protocol and specification..." The wonderful thing about standards is that there are so many to choose from. I suspect that the problem will now be how far manufacturers are…
  • shabaz
    shabaz over 2 years ago in reply to beacon_dave +1
    There should be a national campaign here about the dangers of poor-quality chargers. There are news stories but feel it needs to be more than that, not left to the news websites. Same with e-bikes and…
Parents
  • beacon_dave
    beacon_dave over 2 years ago

    One area that may be of a concern with this future is what happens when things go wrong.

    How is your equipment warranty going to hold out when a fault or incompatibility damages your expensive device that you have just plugged in to recharge. If the manufacturer didn't supply the charger/PSU along with the appliance, then they are likely to just walk away (or rather charge you for an out of warranty repair/replacement).

    Ever since the increase in house fires due to counterfeit phone chargers, fire authorities have been urging consumers to only use the manufacturer supplied charger for the device whilst insurance companies have been walking away. If manufacturers are no longer supplying the charger with the device, then this could be an issue, otherwise you end up back to a drawer full of (more expensive)  chargers again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to beacon_dave

    There should be a national campaign here about the dangers of poor-quality chargers. There are news stories but feel it needs to be more than that, not left to the news websites. Same with e-bikes and chargers. There's a house around the corner with the upstairs burned to a crisp due to an e-bike related fire.. no idea if it was caused by the charger or the batteries or both. Obviously they left it unattended (maybe even overnight! but I'm speculating).

    The average consumer maybe still has no idea what PD with USB-C can provide. I was speaking to a colleague who sells a product which doesn't come with a charger. For his first batch, he offered the customers the choice of a USB type A, or a USB-C cable, with the advice for users to use newer chargers with a USB-C connector. However, the majority of users still opted for the older cable, even though he tried to persuade them that the product would charge faster with USB-C and the latest USB-PD (and it was a more expensive cable, but he was charging the same price). Based on that, I wouldn't be surprised if a lot of phone users still use the cheapest chargers and wonder why it takes all day to charge.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz

    "...Same with e-bikes and chargers..."

    Looks like the UK Office for Product Safety and Standards are finally on the case...

    "...The Office for Product Safety and Standards (OPSS) has today published information for consumers to raise awareness around the safe purchasing, use and charging of e-bikes and e-scooters..."

    https://www.gov.uk/government/news/opss-publishes-consumer-information-on-e-bike-and-e-scooter-battery-safety

    Oh wait... 

    https://www.gov.uk/guidance/my-safety-e-bikes-and-e-scooters-battery-charging

    ...is that it ? A few stickers ?

    More info over at FireEngland Phew!: 

    https://fireengland.uk/fire-safety/charging-your-e-bike-or-e-scooter

    but:

       "Always use the manufacturer-approved battery and charger"

    which USB-PD is effectively trying to doing away with to reduce e-waste so you are back to no-name brand electronic goods that are waltzing past Trading Standards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz

    "...Same with e-bikes and chargers..."

    Looks like the UK Office for Product Safety and Standards are finally on the case...

    "...The Office for Product Safety and Standards (OPSS) has today published information for consumers to raise awareness around the safe purchasing, use and charging of e-bikes and e-scooters..."

    https://www.gov.uk/government/news/opss-publishes-consumer-information-on-e-bike-and-e-scooter-battery-safety

    Oh wait... 

    https://www.gov.uk/guidance/my-safety-e-bikes-and-e-scooters-battery-charging

    ...is that it ? A few stickers ?

    More info over at FireEngland Phew!: 

    https://fireengland.uk/fire-safety/charging-your-e-bike-or-e-scooter

    but:

       "Always use the manufacturer-approved battery and charger"

    which USB-PD is effectively trying to doing away with to reduce e-waste so you are back to no-name brand electronic goods that are waltzing past Trading Standards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 2 years ago in reply to beacon_dave

    Nice!

    I'm sure people routinely check the government's portal for appliance safety, but, and this is just a layman's opinion, there's a slight chance just a few tens of millions might be behind the curve on this.

    Anyway, it is good to see our taxes being used to design these stickers that we can all learn from!!

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz

    I was disappointed that there wasn't one specifically for the element14 site though... just for three of the less popular sites.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to beacon_dave

    There must (may) be some market investigation, that helped them to decide where to advertise?

    Here, they may be preaching to the choir ...