Power & Energy
  • Technologies
  • More
Power & Energy
Blog Vishay microBUCK SiC461 Eval Board
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
  • Author Author: wolfgangfriedrich
  • Date Created: 14 Mar 2021 1:25 AM Date Created
  • Views 1080 views
  • Likes 6 likes
  • Comments 2 comments
  • vishay
  • sic461
  • microbuck® regulators
  • jumpers
Related
Recommended

Vishay microBUCK SiC461 Eval Board

wolfgangfriedrich
wolfgangfriedrich
14 Mar 2021

The Vishay microBUCK eval kit, which was a price I won during the 5 Things to Know About Buck Regulators (Winners Announced: Win a Buck Regulator EV Board for Asking Questions!) webinar, arrived today.

YAY. I had to pay import duty, as the board came from the UK and the paperwork was labeled as a regular invoice. UPS processing fee was higher than the duty itself, but it is OK, the board is definitely worth it.

 

It is a nifty little board featuring the SIC461 wide input voltage, high efficiency synchronous buck regulator with a huge inductor and I am sure it will make its way into one of my future tbd projects.

This is how the board looks like:

image

 

My first observation were the jumpers on the board. In the image above, they look un-suspicious, but only because there is no real reference like a banana for scale.

Here is a detail shot with a regular 0.1" jumper next to them.

image

The jumpers on the board are 0.05" (1.27mm) pitch and they are as tiny as they look in the image. Just pulling or inserting them is a challenge without magnification and tweezers.

As this is a REV A board, my only hope is, that this was an honest footprint mistake, which was missed during layout review because of the lack of scale on the screen. Especially, as there is plenty of real estate on the board for regular sized jumpers. I have to admit, I was not even aware that Hobbit size jumpers exist and I might even use them when I have to do a miniature size layout. But on this board regular jumpers would have been the right choice.

 

I will report about the functionality and performance of the board when I had a chance to test it. until then....

 

PS: Those are the first images I have taken with my new light-box. i am going to describe it in a separate post.

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 5 years ago +2
    Indeed, your board seems to be an entirely different, earlier or perhaps later version, compared to the one I thoroughly RoadTested: Vishay Synchronous Buck Regulator EV Board - Review The converter itself…
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to Gough Lui +2
    Gough Lui A thorough review indeed. Respect! And those jumpers wont go anywhere with their different pitch.
Parents
  • Gough Lui
    Gough Lui over 5 years ago

    Indeed, your board seems to be an entirely different, earlier or perhaps later version, compared to the one I thoroughly RoadTested: Vishay Synchronous Buck Regulator EV Board - Review

     

    The converter itself performs excellently, although the construction of my board was not quite 100%.

     

    At least your board has jumper switchable voltage outputs and includes the jumper shunt itself.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 5 years ago

    Indeed, your board seems to be an entirely different, earlier or perhaps later version, compared to the one I thoroughly RoadTested: Vishay Synchronous Buck Regulator EV Board - Review

     

    The converter itself performs excellently, although the construction of my board was not quite 100%.

     

    At least your board has jumper switchable voltage outputs and includes the jumper shunt itself.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to Gough Lui

    Gough Lui A thorough review indeed. Respect!

    And those jumpers wont go anywhere with their different pitch.image