Power & Energy
  • Technologies
  • More
Power & Energy
Blog XC9145B33CER-G Evaluation Board
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Toptech-Voices
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 24 Jun 2023 12:28 AM Date Created
  • Views 1016 views
  • Likes 8 likes
  • Comments 1 comment
  • XC9145B33CER-G EVB
  • torex dc/dc converter
Related
Recommended

XC9145B33CER-G Evaluation Board

ralphjy
ralphjy
24 Jun 2023

I received a Torex XC9145B33CER-G evaluation board a few weeks ago and thought that I'd try it out.  The EVB PCB is designed for their XC9141/42, XC9145, and XC9147/48 DC/DC converters.  This particular board is fitted with an XC9145B33 which has a 3.3V @ 300mA output.

image

These parts have 3 different footprints available - the PCB is using the USP-6C.

image

I don't think that you could identify the specific converter from the markings - I'll have to label the EVB in case I ever get one with a different converter.

image

The salient specs for this part are the ultra low 400nA quiescent current, and high efficiency (~90%) at low current (<10uA).  I thought this might be a good converter for low duty-cycle battery powered IoT applications.

Torex has a static dc/dc simulator that allows you to plug in various parameters and see the effect for different EVB configurations.  So, I plugged in my EVB and gave it a try.

image

image

I'm interested in using either rechargeable 1.2V NIMH or 1.5V alkaline batteries at loads from 100uA to 30mA and the simulator results looked promising.  The feature I wish the simulator had was to sweep parameters and output plots.

I decided that I would try using my Nordic Power Profiler 2 (ppk2) to take input current measurements while sweeping the input voltage with a fixed output load to get a sense of the range of operation and efficiency at various loads.  I decided to sweep from 1V to 3.3V in 100mV steps.  I used loads of 100uA, 1mA, 10mA, and 20mA.  I was intially surprised with the response, but it was somewhat repeatable.

100uA

imageimage

1mA

imageimage

10mA

imageimage

20mA

imageimage

I repeated the sweeps at 100uA and 1mA and also plotted the simulator response.

image

image

I mentioned this to the Torex rep and he pointed out the spec for this part calls out a "start voltage" of 1.6V

image

There is a "Chip Enable" for this part that enables the converter.  I had tied it to the input voltage based on what I saw in this table

image

But futher down the spec

image

So there isn't a guaranteed enable until CE is above 1.5V - hence the start voltage of 1.6V.  I went back and observed the output voltage and sure enough it was not at 3.3V  when I was getting the funny current values at the lower input voltages.

The funny current values when the input voltage is close to the output voltage is a different effect, but it would not have affected me because I did not intend to operate at those voltages - just wanted to see what the part would do - BTW the output stayed at 3.3V even with the input current moving around.

Anyway, this part won't work for what I wanted.  Torex has other parts (XC9140, XC9110/9111) that are intended for lower voltage inputs that are 10-15% less efficient, but are designed to work with NIMH and alkaline batteries (start voltage ~0.9V).  I'm not sure where the simulator puts the CE voltage as that is not a parameter that you can change.  

  • Sign in to reply
Parents
  • DAB
    DAB over 3 years ago

    Nice post.

    Yes reading the fine print is very important in selecting your devices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 3 years ago

    Nice post.

    Yes reading the fine print is very important in selecting your devices.