Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging two 3.7v Li-Ion Cells
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 287 subscribers
  • Views 6032 views
  • Users 0 members are here
  • series
  • lithium
  • 7.4
  • 3.7
  • charger
Related

Charging two 3.7v Li-Ion Cells

e14 Contributor
e14 Contributor over 11 years ago

So for a portable project, I will be using two lithium ion 2200mah 3.7v batteries in series to give me 7.4v. I have a USB powered 3.7v Lithium Ion charger found here https://www.adafruit.com/products/1905 . How could I charge both the batteries in parallel and then use them in series for 7.4v?

 

All help is greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to dougw +2
    I see some problems with this idea - if one battery is at a significantly different state of charge and thus voltage form the other (and this happens as the batteries age) then a huge current will flow…
  • Kilohercas
    Kilohercas over 11 years ago in reply to derkarhu +1
    You can also make very expensive circuit for battery charging, with CCCV push/pull 3A converters, just treat them as capacitors http://cds.linear.com/docs/en/datasheet/8052ff.pdf Super-capacitors are equivalent…
Parents
  • lz1ppl
    lz1ppl over 11 years ago

    You ca just use something like that:

    http://www.ebay.com/itm/2pcs-2-Cell-Lithium-Battery-Charging-Board-Charger-Module-Protection-DC-7-4V-3A-/151715735343?pt=LH_DefaultDomain_0&hash=item2352f6672f

    or that:

    2 Cells Single Lithium ion Battery Charger Module 1 2A PCB 18650 TP5100 iPhone | eBay

     

    Or if you want to do it yourself you can use MCP73213 http://ww1.microchip.com/downloads/en/DeviceDoc/20002190C.pdf or some similar product.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to lz1ppl

    i know this is a little old now but does anyone know if this is balancing?

     

    2 Cells Single Lithium ion Battery Charger Module 1 2A PCB 18650 TP5100 iPhone | eBay

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mkhanemkay
    mkhanemkay over 8 years ago in reply to e14 Contributor

    Hi,

     

    I have the same question, did you ever find the answer, could you kindly reply if you figured out if it balances or a Balance board is necessary.

     

    Also, do you happen to know if we can charge 2s @ 5v input with this? , as this one seems like a switching type module (probably doing buck ,maybe)...

     

    Thanks,

    Khan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mkhanemkay
    mkhanemkay over 8 years ago in reply to e14 Contributor

    Hi,

     

    I have the same question, did you ever find the answer, could you kindly reply if you figured out if it balances or a Balance board is necessary.

     

    Also, do you happen to know if we can charge 2s @ 5v input with this? , as this one seems like a switching type module (probably doing buck ,maybe)...

     

    Thanks,

    Khan