Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging two 3.7v Li-Ion Cells
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 287 subscribers
  • Views 6012 views
  • Users 0 members are here
  • series
  • lithium
  • 7.4
  • 3.7
  • charger
Related

Charging two 3.7v Li-Ion Cells

e14 Contributor
e14 Contributor over 11 years ago

So for a portable project, I will be using two lithium ion 2200mah 3.7v batteries in series to give me 7.4v. I have a USB powered 3.7v Lithium Ion charger found here https://www.adafruit.com/products/1905 . How could I charge both the batteries in parallel and then use them in series for 7.4v?

 

All help is greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to dougw +2
    I see some problems with this idea - if one battery is at a significantly different state of charge and thus voltage form the other (and this happens as the batteries age) then a huge current will flow…
  • Kilohercas
    Kilohercas over 11 years ago in reply to derkarhu +1
    You can also make very expensive circuit for battery charging, with CCCV push/pull 3A converters, just treat them as capacitors http://cds.linear.com/docs/en/datasheet/8052ff.pdf Super-capacitors are equivalent…
Parents
  • derkarhu
    derkarhu over 11 years ago

    Normal charge voltage for a 3.7 V Li-ion cell is 4.2 V _during_ the main charge, BUT only if the cell is within a normal charge temperature, above 0°C and <+40 (not sure about the maximum, please check that), and a 'float voltage of 3.8 to 3.9 V.

     

    If you simply apply 3.7 V per cell, you will not charge the battery most efficiently, and will not get the cell(s) to their full charge state...the fully-charged state is quite a bit above the nominal 3.7 V cell voltage, which is actually the rated voltage witha load applied. Fully-charged, with no load, the Li-ion cell will be > 3.9 V 'open circuit'

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • derkarhu
    derkarhu over 11 years ago

    Normal charge voltage for a 3.7 V Li-ion cell is 4.2 V _during_ the main charge, BUT only if the cell is within a normal charge temperature, above 0°C and <+40 (not sure about the maximum, please check that), and a 'float voltage of 3.8 to 3.9 V.

     

    If you simply apply 3.7 V per cell, you will not charge the battery most efficiently, and will not get the cell(s) to their full charge state...the fully-charged state is quite a bit above the nominal 3.7 V cell voltage, which is actually the rated voltage witha load applied. Fully-charged, with no load, the Li-ion cell will be > 3.9 V 'open circuit'